Is there a simple and fast way to be able to select between writing the microcontroller for Debug or for production (read and delete protection).
I already found out that by configuring the last byte of Flash_Config in the startup file I can program the microcontroller with read and delete protection. The problem is that having to change this byte by hand every time I want to switch between development doing Debug and production with read and delete protections is not comfortable at all.
Solved! Go to Solution.
Yes, the build configuration sets all the build options/etc.
So you can have two builds, with:
- Develop, this one has the define set with option -D, for example BUILD_FOR_PRODUCTION=0
- Production, this one has set BUILD_FOR_PRODUCTION=1
Then in your startup file you have this:
__attribute__ ((used,section(".FlashConfig"))) const struct {
    unsigned int word1;
    unsigned int word2;
    unsigned int word3;
    unsigned int word4;
} Flash_Config = 
#if BUILD_FOR_PRODUCTION==1
{0xFFFFFFFF, 0xFFFFFFFF, 0xFFFFFFFF, whatever you put here }; /* flash security enabled */
#else /* debug/develop */
{0xFFFFFFFF, 0xFFFFFFFF, 0xFFFFFFFF, 0xFFFFFFFE};
#endif
That way you have the full flexibility, and you can use that macro in other places too (e.g. for extra logging, etc).
I hope this helps,
Erich
Have you considered using Build Configurations (https://mcuoneclipse.com/2016/05/19/build-configurations-in-eclipse/ ) for this?
You could have a 'develop' and a 'release' configuration with just different settings (e.g define) or file included/excluded.
I hope this helps,
Erich
Thanks.
But I think that's just for build configuration parameters, where I don't see the state of the bits to protect the microcontroller against reading or erasing.
I think that if I define a constant with #define and put an #ifdef in the startup file, I could select that various settings of these bits are applied. Although I'm not really sure if the #defines put in my sources will affect the startup file as well or I put it directly in the startup file.
Yes, the build configuration sets all the build options/etc.
So you can have two builds, with:
- Develop, this one has the define set with option -D, for example BUILD_FOR_PRODUCTION=0
- Production, this one has set BUILD_FOR_PRODUCTION=1
Then in your startup file you have this:
__attribute__ ((used,section(".FlashConfig"))) const struct {
    unsigned int word1;
    unsigned int word2;
    unsigned int word3;
    unsigned int word4;
} Flash_Config = 
#if BUILD_FOR_PRODUCTION==1
{0xFFFFFFFF, 0xFFFFFFFF, 0xFFFFFFFF, whatever you put here }; /* flash security enabled */
#else /* debug/develop */
{0xFFFFFFFF, 0xFFFFFFFF, 0xFFFFFFFF, 0xFFFFFFFE};
#endif
That way you have the full flexibility, and you can use that macro in other places too (e.g. for extra logging, etc).
I hope this helps,
Erich
Ok, perfect, thank you very much.