Why does MCUXpresso IDE not filter out incompatible SDK versions?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why does MCUXpresso IDE not filter out incompatible SDK versions?

2,116 Views
abnxpweb
Contributor III

Hi,

In older releases of MCUXpresso IDE, the IDE would filter out newer, incompatible versions of the SDKs in the "Install MCUXpresso SDKs" view. But this functionality broke some time ago, and now the view seems to show the latest versions, even when they won't work with my IDE.

This is really annoying when I am still using an old release of MCUXpresso IDE for various project reasons, after NXP have released new SDK & IDE versions that I am not yet ready to move onto.

And if I am not very careful I end up trying to install a newer SDK than my IDE can cope with - the IDE then seems to half install it, but fail to make it usable, whilst blocking the installation of an older SDK version until I can work out how to actually uninstall the broken install of the newer one.

For example I today needed to use an LPC845 with my MCUXpresso IDE v11.5.1 install. And the "Install MCUXpresso SDKs" views offers me v2.12.0, rather than v2.11.0 which would work.

I assume some versioning check in the IDE has broken. Or else maybe the SDK version numbers are no longer being updated in the way the IDE expects.

Anyway, this always used to work - please make it do so again! Otherwise you are leaving it up to me the user to try and work out what IDE and SDK version are compatible with each other - not a nice user experience!

Thanks, AB

0 Kudos
Reply
5 Replies

2,101 Views
abnxpweb
Contributor III

Thanks Jennie - but unfortunately it doesn't help.

I am highlighting a defect with the IDE and SDK that functionality that used to work to ensure that only compatible SDKs were displayed in the IDE's Install MCUXpresso SDK view is now broken.

It should not be down to me as a user to have work out what SDKs are compatible when using this view - which is the primary way NXP is driving customers to use to install SDKs. Especially given that by default the view only shows the latest ones which are incompatible with the IDE version I am using.

I should not be seeing SDK v2.12 list in the view in an IDE version that only supports SDKs up to v2.11. As I said, this all used to work. Please raise with the IDE team to get it to work again.

0 Kudos
Reply

2,094 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Could you please send me screenshot of "IDE and SDK that functionality that used to work to ensure that only compatible SDKs were displayed in the IDE's Install MCUXpresso SDK view"

I will query it with SW team why it was removed and possibility of adding it back.

Thanks,

Jun Zhang

0 Kudos
Reply

2,073 Views
abnxpweb
Contributor III

From experimentation, it looks like the issue is in the data stored in the SDK system, not the IDE. So I can't give you a screenshot from the IDE viewpoint.

The IDE should know what the latest version of the SDK it can load is, from a version number in the tag in the xml. It looks to me at some point like the SDK system has stopped updating this number - and hence the IDE is assuming it can load all of the available SDK versions from the web system.

0 Kudos
Reply

2,059 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

OK. Will forward it as a customer requirement to SW team.

For now, please use the method in my first reply to manage SDK version for specific IDE.

Thanks,

Jun Zhang

0 Kudos
Reply

2,105 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi abnxpweb 

MCUXpresso IDE version must match SDK versions.

In SDK package readme file, we can see which version of IDE is suggested for this versions of IDE.

For a certain version of IDE, I suggest you installing all the supported SDK versions to a defined folder to make sure SDK and IDE versions match.

ZhangJennie_0-1659427429797.png

 

Hope this helps,

Jun Zhang

 

0 Kudos
Reply