Why does MCUExpresso IDE v10.1.1 compile so slow compared to v10.0.2?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why does MCUExpresso IDE v10.1.1 compile so slow compared to v10.0.2?

910件の閲覧回数
johnsorensen
Contributor II

The build is very slow after newly installing v10.1.1. I am connected to a Rigado R41Z board.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

708件の閲覧回数
johnsorensen
Contributor II

Today, everything looks as it should and the build(compile) time of each system are about equivalent, that is about 35 seconds now after a Clean using 24_OpenSDA_FRDM-KW41Z.bin. I had just updated to the latest SDK_2.x_FRDM-KW41 2.2.0  with both IDE v10.0.2 and v10.1.1 loaded. I most likely had a many other applications running also. So not exactly sure why this happened, but working fine now and with both systems loaded. Host  is Windows 7 Professional. Hardware - a Dell Precision M4700.

0 件の賞賛
返信

708件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

We certainly would not expect to see any major differences in the time taken to build projects in the two releases. And we have not received any customer reports of this either.

What host OS are you running on? And if you do a clean, then build of your project, on both IDE versions - what sort of build times are you seeing?

Note - the usual suspect in these sorts of situations is virus protection software.

Regards,

MCUXpresso IDE Support

0 件の賞賛
返信