What is difference between evkmimxrt1170 and evkbmimxrt1170 SDK?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What is difference between evkmimxrt1170 and evkbmimxrt1170 SDK?

跳至解决方案
3,345 次查看
simmania
Contributor III

Hi,

I have the MIMXRT1170-EVK board. When making an SDK for it, I can choose between evkmimxrt1170 and evkbmimxrt1170. What is the difference? When to choose which one?

 

0 项奖励
回复
1 解答
3,332 次查看
Miguel04
NXP TechSupport
NXP TechSupport

Hi @simmania 

The EVKB is the second version that include erratas fixes. I recommend you to use this revision (EVKB).

Best Regards, Miguel.

在原帖中查看解决方案

0 项奖励
回复
6 回复数
1,426 次查看
Littell
Contributor III

Sometimes you guys (NXP) are really good at NOT answering questions:

  Why do images built with the RT1170 EVK SDK not run on a RT1170 EVKB (and vice versa)?

0 项奖励
回复
3,288 次查看
simmania
Contributor III

Correction:
evkmimxrt1170 and evkbmimxrt1170 seem to be for different boards. I have the MIMXRT1170-EVK board, so I need the evkmimxrt1170. When using the evkbmimxrt1170, I get strange errors.

0 项奖励
回复
3,276 次查看
Miguel04
NXP TechSupport
NXP TechSupport

Thanks for the correction, I assumed you were using revision B from the RT1170.

Best Regards, Miguel.

0 项奖励
回复
3,333 次查看
Miguel04
NXP TechSupport
NXP TechSupport

Hi @simmania 

The EVKB is the second version that include erratas fixes. I recommend you to use this revision (EVKB).

Best Regards, Miguel.

0 项奖励
回复
2,986 次查看
sparky34
Contributor I

Hi, is there a document somewhere that outlines what Errata are fixed in MIMXRT1170-EVKB (vs. MIMXRT1170-EVK)?  A design we have in process was originally based on the MIMXRT1170-EVK and I want to make sure that we incorporate any fixes in MIMXRT1170-EVKB.  Also, code that we had compiled for the EVKB is not running at all on the EVK so we'd like to know what the specific hardware differences are.

0 项奖励
回复
2,474 次查看
anthony_huereca
NXP Employee
NXP Employee

Here are the differences between the i.MX RT1170  EVK and i.MX RT1170 EVKB:

 

anthony_huereca_0-1701811430227.png

 

There is a EVKB Hardware User Guide that includes this table coming out soon. It is recommended that any new users to RT1170 use the EVKB board as it is the newer board and includes more features as you can see above. 

Also per the original question, make sure to download the correct SDK for your version of the board:

i.MXRT1170 EVK: SDK_2_14_0_MIMXRT1170-EVK

i.MX RT1170 EVKB: SDK_2_14_0_MIMXRT1170-EVKB

 

 

0 项奖励
回复