Using a PNEV7462 with a 3.3V supply.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using a PNEV7462 with a 3.3V supply.

993件の閲覧回数
rich3
Contributor II

I am evaluating the PNEV7462. I have successfully compiled and run the example projects using the 5V supply.

I have set the board to the 3.3V supply by switching the JP5 jumper to 3V3. I am now unable to debug the projects.

I am using the LPCLink 2 and MCU Xpresso.

The errors include:

Failed to execute MI command.

Error finishing flash operation.

Target error from Commit Flash write: EP(08). Cannot access cor regs when target running.

GDB protocol problem.

Can you please point me in the right direction?

Thanking you in advance.

タグ(2)
0 件の賞賛
返信
1 返信

933件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

May I ask if you are working with the green board or black board?

Regards,

Ivan.

0 件の賞賛
返信