Update MCUXpresso IDE keeping SDK's

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Update MCUXpresso IDE keeping SDK's

Jump to solution
4,853 Views
bwinter
Contributor II

I'm learning to use and get used to MCUXpresso by testing it on a small test project a LPC845-BRK.

I started with MCUXpresso IDE v11.2.0_4120, installed a few SDK's (LPC845BREAKOUT, LPCXpresso.. )

However i yesterday updated to MCUXpresso IDE v11.2.1_4149 by downloading the package and installing it. New version in parallel to existing version.

However on starting the new version all SDK's are gone!

Do i have to install all SDK's again each time an update is done (approx 4 times a year)?
At the moment i only have 2 installed but once we make te full transition to MCUXpresso multiple machines will need the update.

Is installing a new version of MCUXpresso to a general directory (without version number)(eq C:\ nxp\MCUXpressoIDE\ ) recommended and would that keep all installed SDK's?

Tags (2)
1 Solution
4,777 Views
ErichStyger
Specialist I

Hi @bwinter ,

not sure what it is. To my understanding the path naming with  "....\mcuxpresso\02\SDKPackages" has been introduced to keep up with SDK version changes.

Have you tried to import (drag&drop) the SDK(s) into the new version? Maybe this fixes it?

 

I hope this helps,

Erich

View solution in original post

0 Kudos
Reply
7 Replies
4,821 Views
abnxpweb
Contributor III

If you installed your SDKs using the "Plugin SDK" mechanism, so directly installing them from within the IDE itself, then the SDK are effectively standard Eclipse plugins. Thus they can be imported from an old install of the IDE to your new one using the Eclipse plugin import mechanism described in the IDE's Installation Guide ....

To do this, from your new installation select File -> Import -> Install -> From Existing
Installation and point at the ide directory within your original IDE’s installation directory. Note:
that on macOS / Linux – this option will effectively run automatically the first time you run the
new version of the IDE.

Of course, you might want to instead take the opportunity to also update to a newer version of the SDK that may be available for use with the newer version of the IDE.

Hope this helps!

Tags (1)
4,810 Views
bwinter
Contributor II

abnxpweb , Tried you suggestion but got stuck on to which directory i have to point.

message: Specify the path to a valid application installation. Error remains on all paths.

paths tried: C:\nxp\MCUXpressoIDE_11.2.0_4120  (and some sub.paths)
and path from SDK (which is an empty directory)

EDIT:
i tried "C:\nxp\MCUXpressoIDE_11.2.0_4120\ide" and got the option!
selected both SDK and they got copied and after a reboot appear in my new IDE.

Conslusion: is that SDK need to be installed or copied for every new IDE installation.

This is different from the way ErichS describes as he seems to keep one version of each SDK installed, they way i would prefer.

0 Kudos
Reply
4,789 Views
abnxpweb
Contributor III

Yes, as the IDE's Installation Guide text implies (though I agree you could misread this), you have to point at the actual "ide" subdirectory within the installation directory.

Of course, as Erich points out there are other ways of installing and handling SDKs - but you were asking about the plugin SDK system, which I think you now have a migration solution for.

There is lots more information on the various options for installing SDKs contained within the IDE's User Guide if you want to look further into what Erich suggests - so you might want to read that too.

[TBH - its a bit annoying that NXP haven't updated their User Guide to explicitly cover the migration of plugin SDKs from one version to another.]

Anyway, hope this helps!

0 Kudos
Reply
4,843 Views
ErichStyger
Specialist I

Hi @bwinter ,

I have done the same (installing new IDEs (of course in different folders) and it kept the previously installed SDKs as they are shared between the IDEs. If you have many SDKs, it takes a few minutes to list them in the View.

If not: try to do a refresh if this helps?

ErichS_0-1605855994780.png

Check the SDK preferences:

ErichS_1-1605856047675.png

And it should show you the SDK location:

ErichS_2-1605856074500.png

Can you check this?

I hope this helps,

Erich

0 Kudos
Reply
4,812 Views
bwinter
Contributor II

ErichS, thanks for your help.

I did the refresh -> no difference.
Took a look at the SDK location the way you described. -> both installs have exact the same path and all settings are exact the same as the ones in your picture. The only difference is of course my username is different.

I then went to the mentioned directory: "....\mcuxpresso\02\SDKPackages". the directory is empty!?

I do have SDK's installed.
Two under my old "MCUXpresso IDE v11.2.0_4120" version and
One (installed yesterday through IDE install SDK because i wanted to continue) in my new "MCUXpresso IDE v11.2.1_4149" version.

The two SDKs from the old version are still not available in  the new version.
(tried the option from the post by abnxpweb but got stuck on to which directory i have to point)

0 Kudos
Reply
4,778 Views
ErichStyger
Specialist I

Hi @bwinter ,

not sure what it is. To my understanding the path naming with  "....\mcuxpresso\02\SDKPackages" has been introduced to keep up with SDK version changes.

Have you tried to import (drag&drop) the SDK(s) into the new version? Maybe this fixes it?

 

I hope this helps,

Erich

0 Kudos
Reply
4,731 Views
bwinter
Contributor II

Hi Erich

it's getting clear now.
Evaluating MCUXpresso on two systems (Work-Work & Work-Home) and using both types of SDK's (download & plugin) without knowing the differences together with using the downloaded versions for another compiler made it a little unclear

Seems i mainly messed up the 2 types of SDK's, the "Classic" Filesystem SDK's and the Plugin SDK's.
Both methods now work perfect. Download+Drag&Drop moves it to the right path and makes the SDK available for every installed version.

The Plugin SDK's can be used from other installs by using the method described by abnxpweb and selecting the correct path.

 

0 Kudos
Reply