I'm learning to use and get used to MCUXpresso by testing it on a small test project a LPC845-BRK.
I started with MCUXpresso IDE v11.2.0_4120, installed a few SDK's (LPC845BREAKOUT, LPCXpresso.. )
However i yesterday updated to MCUXpresso IDE v11.2.1_4149 by downloading the package and installing it. New version in parallel to existing version.
However on starting the new version all SDK's are gone!
Do i have to install all SDK's again each time an update is done (approx 4 times a year)?
At the moment i only have 2 installed but once we make te full transition to MCUXpresso multiple machines will need the update.
Is installing a new version of MCUXpresso to a general directory (without version number)(eq C:\ nxp\MCUXpressoIDE\ ) recommended and would that keep all installed SDK's?