Undefined reference in one function; other functions are fine

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Undefined reference in one function; other functions are fine

Jump to solution
42,766 Views
chadgraham
Contributor V

Hello,

I have a very large project that consists of numerous libraries and a ThreadX RTOS application.  In one of the libraries, I have a C++ class that handles mutexes and I can compile that library without issues.  However, when I compile the code application, I get an error "undefined reference to `_txe_mutex_info_get'".

I have double checked the includes, the include paths, the libraries, the library paths, but everything seems correct.  (Commenting out the "tx_mutex_info_get()" function call kills the error.)  To make it more frustrating, both the library and the application code have been playing nice for over a year and the function call "tx_mutex_info_get()" is used in other functions in the same class without errors.  I've walked all of the changes I've made since the last compile, but that too has proven unfruitful.

Does anyone have any suggestions?

UINT RtController_Mutexes::_getMutexOwner(
TX_MUTEX * mutex,
TX_THREAD ** owner)
{
UINT status;
std::string msg;
CHAR ** name = NULL;
ULONG * count = NULL;
TX_THREAD ** first_suspended = NULL;
ULONG * suspend_count = NULL;
TX_MUTEX ** next_mutex = NULL;

status = tx_mutex_info_get(
mutex,
name,
count,
owner,
first_suspended,
suspend_count,
next_mutex);

// Check for log file controller creation error.
if( status != TX_SUCCESS)
{
// Error stuff
} else
return( status);
}

 

0 Kudos
Reply
1 Solution
42,747 Views
ErichStyger
Specialist I

'undefined reference' means that you are calling that method/function/object, but the linker cannot find it.

A few things to check:

- is txe_mutex_info_get called with C or C++ name mangling? It could be that it has been compiled with C++, but you are calling it with C naming? (note: extern "C")

- use the IDE image info: is that object in question present in the binary or not?

- provide a dummy/empty txe_mutex_info_get() in your application, just to make the linker happy. Then check the map file what happend with the one from the OS

- are you using higher level of optimizations? I have seen cases with some 'not so clean code' where the compiler/linker have removed objects, which had lead to such errors

 

I hope this helps,

Erich

View solution in original post

2 Replies
42,748 Views
ErichStyger
Specialist I

'undefined reference' means that you are calling that method/function/object, but the linker cannot find it.

A few things to check:

- is txe_mutex_info_get called with C or C++ name mangling? It could be that it has been compiled with C++, but you are calling it with C naming? (note: extern "C")

- use the IDE image info: is that object in question present in the binary or not?

- provide a dummy/empty txe_mutex_info_get() in your application, just to make the linker happy. Then check the map file what happend with the one from the OS

- are you using higher level of optimizations? I have seen cases with some 'not so clean code' where the compiler/linker have removed objects, which had lead to such errors

 

I hope this helps,

Erich

42,710 Views
chadgraham
Contributor V

Thanks Erich!  I was able to determine that the functions were in the library, but the functions were indeed mangled.  I ended up revamping the includes and added "extern "C"" to the "#include" statements and I'm moving forward again.  Thanks!

0 Kudos
Reply