I'm trying to add PAN ID ,profile and cluster to a JN5189 project using the ZigBee Pro (ZBPro) Configuration Editor in MCUXpresso, but I'm unable to set the value . As soon as I enter a value, then leave the text box, the value wont change it remains unchanged.
Solved! Go to Solution.
Hi @logum4,
The Zigbee stack is based on the specification, it generates randomly the PAN ID to avoid any PAN ID conflict. Unfortunately, it is not possible to set the PAN ID by the user.
Regards,
Mario
Hi @logum4,
The Zigbee stack is based on the specification, it generates randomly the PAN ID to avoid any PAN ID conflict. Unfortunately, it is not possible to set the PAN ID by the user.
Regards,
Mario
Hii Mario,
its correct that randomly generates the PAN ID to avoid any PAN ID conflict but if we use more than 2 groups at a time then there PAN ID should be different ?
what are the parameters should be defined if we use more than 2 groups at a time?