Hi.
The IDE reports that the configuration tools (pin, clock, peripherals, etc.) for part MIMXRT117HDVMAA are not available. Any workaround available or just wait for an update?
The project was created based on the SLN-VIZN3D-IOT board and the SDK_2.x_SLN-VIZN3D-IOT, as indicated in the tutorial.
Using the latest IDE version 11.7.1 [Build 9221] [2023-03-28]
Thanks.
Hello, I review the information on this, and I suggest using any example for the RT1170 because the name of the solution is RT117H, but this maybe has an RT1176.
Or in another ay with the Config Tool Standalone, you could try to configure and then you can import that to your project.
Best regards,
Pavel
Hello, my name is Pavel, and I will be supporting your case, let me get into your case and when I have more information, I will contact you.
Best regards,
Pavel