Unable to connect LPC Link-2 to LPC54606 using SWD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to connect LPC Link-2 to LPC54606 using SWD

ソリューションへジャンプ
3,330件の閲覧回数
hemanthvasista
Contributor IV

Hello ,

I am unable to connect LPC Link-2 to NXP LPC54606 controller.

SWDIO (PIO0_12) with pullup to LPC Link-2 (J7 pin-2)
SWO (PIO0_8) with pullup to LPC Link-2 (J7 pin-6)
SWCLK (PIO0_11) with pulldown to LPC Link-2 (J7 pin-4)
RESETN with pullup to LPC Link-2 (J7 pin-10)

1. Are there any other conditions that needs to be considered?
2. SWO can be PIO0_8 or PIO0_10, should any configuration be done by user?
3. What should be the state of ISP0, ISP1 & ISP2 pins? (All these pins are pulled up)


regards,
Hemanth

タグ(3)
0 件の賞賛
返信
1 解決策
3,268件の閲覧回数
hemanthvasista
Contributor IV

 

The issue was because of the existing code in the flash which configured the SWD pins as Analog Pins.

Erasing of the flash and then SWD interface started to work.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,297件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello hemanthvasista,

 

You can also have a look at the schematic about LPCpresso54628 board:

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc... 

 

 

0 件の賞賛
返信
3,322件の閲覧回数
converse
Senior Contributor V
0 件の賞賛
返信
3,319件の閲覧回数
hemanthvasista
Contributor IV

I tried the things described in the that link without any success

0 件の賞賛
返信
3,306件の閲覧回数
converse
Senior Contributor V

Check power. And double check your debug connections.

0 件の賞賛
返信
3,269件の閲覧回数
hemanthvasista
Contributor IV

 

The issue was because of the existing code in the flash which configured the SWD pins as Analog Pins.

Erasing of the flash and then SWD interface started to work.

0 件の賞賛
返信