Terminate and Relaunch a debug session not possible since Upgrade to MCUXpresso v11.1.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Terminate and Relaunch a debug session not possible since Upgrade to MCUXpresso v11.1.1

跳至解决方案
2,586 次查看
nobodyKnows
Contributor III

Hello,

the "Terminate and Relaunch" of a debug session result in the following error "There is already a running debug session for the launch configuration". It is not possible to kill this running debug session.

I have to restart MCUXpresso to get it work again. The only way to kill this debug session without restarting is using "Terminate and Remove".

I am using Linux with the lastest MCUXpresso IDE v11.1.1 [Build 3241] [2020-03-02] and a Segger debugger.

I hope someone have a hotfix for this issue.

Thanks a lot and best reagards,

Maximilian

0 项奖励
回复
1 解答
2,416 次查看
nxf58474
NXP Employee
NXP Employee

Hi,

 

Could you please try to delete your Launch configuration? With this you put the debug connection settings back to the default.

 

Regards,

Ricardo

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,416 次查看
nxf58474
NXP Employee
NXP Employee

Hi Maximilian,

 

Hope you are doing well. Did you tried the "Terminate all debug sessions" button?

 

Also you can use the "Clean up debug" button, it will kill all debug processes associated with the debug connections.

 

Best Regards,

Ricardo

0 项奖励
回复
2,416 次查看
nobodyKnows
Contributor III

Hello,

"Clean up Debug" has no effect.

"Terminate all debug sessions" button leads to an error and has no effect on the issue.error_term_all.png

I've updated/reinstalled my system to debian 10 but the issue is not solved.

This behavior is really annoying. I hope someone can help me.

0 项奖励
回复
2,417 次查看
nxf58474
NXP Employee
NXP Employee

Hi,

 

Could you please try to delete your Launch configuration? With this you put the debug connection settings back to the default.

 

Regards,

Ricardo

0 项奖励
回复
2,416 次查看
nobodyKnows
Contributor III

Thanks a lot! This was the solution. :smileyhappy:

0 项奖励
回复