Source code of MCUXpresso IDE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Source code of MCUXpresso IDE

2,433 次查看
Mahajna
Contributor I

Hi,

I am using MCUXpresso IDE 11.0.0, I would like to ask if there is a way to reach the source code of it ?

I am working with GIT system that doesn't allow to upload binary files !
I am thinking to upload the source code, then to compile and then to use !

 

Thanks in advance.

0 项奖励
回复
4 回复数

2,309 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

My understanding is that you're asking for source code associated with the EGit plugins available inside the MCUXpresso IDE. That should not be difficult to find - see https://git.eclipse.org/r/plugins/gitiles/egit/egit or/and https://github.com/eclipse-egit 

Note that Eclipse-related source code is mostly open-source (EPL licensed) and can be easily inspected by browsing specific repositories. However, MCUXpresso-specific components are based on proprietary source code.

Not sure about the actual limitations you met but I suggest you switch to the latest MCUXpresso IDE (v11.8.1 available, v11.9.0 to be announced soon) that also comes with newer EGit plugins.

Regards,
MCUXpresso IDE Support

0 项奖励
回复

2,390 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Mahajna 

Do you asked how to use git with MCUXpresso IDE?

If yes, you can refer to EGit User Guider, open from MCUXpresso IDE as below:

Alice_Yang_0-1704248075248.png

 

BR

Alice

 

0 项奖励
回复

2,384 次查看
Mahajna
Contributor I

Hi @Alice_Yang 

Thank you for your reply

This is not what I meant, I asked if there is any way to get the source code of MCUXpresso IDE ?
In other words, is MCUXpresso IDE an open source ?

Thanks in advance.

0 项奖励
回复

2,379 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Mahajna 

Sorry, no.

 

BR

Alice

0 项奖励
回复