Setting a breakpoint halts the system

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Setting a breakpoint halts the system

1,846件の閲覧回数
Daan
Contributor III

Hi,

Whenever my system is running (RT1064 core) and I want to set a breakpoint in runtime, the system halts for a few seconds, after this, normal operation is continued, however, the system has become useless, since other CAN devices missed the heartbeat of the controller. Isn't there a way to set and remove breakpoints transparently?

Cheers,

Daan

0 件の賞賛
返信
2 返答(返信)

1,828件の閲覧回数
Daan
Contributor III

Okay, thank you Erich, I got it. Unfortunately our code is too big to fit in RAM only, so that's not an option, we'll just have to deal with it...

Daan

0 件の賞賛
返信

1,838件の閲覧回数
ErichStyger
Specialist I

Hi Daan,

How breakpoints are set, depends on your debug probe technology. For example the SEGGER J-Link is very fast and is able to reprogram the flash page with a software breakpoint. However, this kind of things requires the target to be halted, programming the flash and then continue.

The other way is to use hardware breakpoints: but this still requires the target to be halted afik.

For an explanation how breakpoints work, see https://mcuoneclipse.com/2012/07/29/software-and-hardware-breakpoints/

The only way to get around this is that the debugger is only able to read/write the RAM memory while the target is running, using some bus free cycles. So you would only be able to do this if your code is running in RAM instead of FLASH.

I hope this helps,

Erich

0 件の賞賛
返信