Segger J-Link does not support iMX8MM M4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Segger J-Link does not support iMX8MM M4

987 Views
davidvescovi
Contributor V

So after being lied too that MCUXpresso IDE support the i.MX8 M4.  I went through the Linux documentation step by step. After much struggling I was able to cross compile the SDK's M4 examples using the stand alone GCC toolchain and cmake.

I then tried to load it via jtag as per the instructions. It shows j-link 6.22 (see attached). I have 6.44a … the latest   It does NOT have the target selection "MIMX8MM6_M4".

As a matter of fact I do NOT see ANY i.MX8 M4 targets?

What gives?

Tags (1)
0 Kudos
1 Reply

741 Views
igorpadykov
NXP Employee
NXP Employee

Hi David

one can try to install segger patches from below link

i.MX Software | NXP 

pastedImage_2.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos