Schematic for IMXRT1050-EVKB Development Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Schematic for IMXRT1050-EVKB Development Board

Jump to solution
4,552 Views
trailerman
Contributor I

Looking for schematics for IMXRT1050-EVKB. The latest version on the NXP site does not seems to match my board.
The board is marked with IMXRT1050-EVKB, however there is a sticky white label on the board with the number SCH-30168 REV A1

What is the significance of EVKB and SCH-30168 REV A1

Not sure if I have the right schematics?

0 Kudos
Reply
1 Solution
4,526 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @trailerman ,

Please see the revision history table in schematic head.

jingpan_0-1650956650813.png

Besides that, the chip is changed from MIMXRT1052DVL6A to MIMXRT1052DVL6B.

 

Regards,

Jing

 

View solution in original post

0 Kudos
Reply
10 Replies
4,381 Views
jvdstoel
Contributor I

Hi Jing,

Things are getting more clear. We have 2 boards: one with rev A cpu, one with rev B cpu. The board with rev B cpu is EVKB version A1. This board has transistor solution for SD card power switch. According to the (only) schematics we have, EVKB version B1 has the new solution. This difference is not documented in the Description of the Revision History. Are there more differences which are undocumented? Or can you arrange a B1 board for me?

I am preparing a hardware design for my product and want to make sure I have all the improvements included in this design.

Why should I, for example, choose for the chip solution instead of the transistor solution? It would be helpful to get some guidance.

Regards,

Johan

0 Kudos
Reply
4,368 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @jvdstoel ,

I think there won't be more different.

The new circuit is to simplify the design I think. It is not complex and just want to switch the power when power on or at any time by MCU.

 

Regards,

Jing

0 Kudos
Reply
4,471 Views
jvdstoel
Contributor I

Hi Jing,

Unfortunately your answer is not correct. I have a new board with REV A1 printed on it. This board contains for example 2 transistors Q7 and Q8 which I cannot find in the schematic diagram. It looks like these are used instead of U37 (SD card power switch). Hopefully the updated documentation is made available soon.

Best regards,

Johan

0 Kudos
Reply
4,465 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @jvdstoel ,

the two transistors can be found on that schematic sheet 4.

jingpan_0-1651897077644.png

 

Regards,

Jing

 

0 Kudos
Reply
4,456 Views
jvdstoel
Contributor I

Hi Jing,

This confirms my point. There are major (?) undocumented differences between the several schematics and pcbs.

The design files on your websites show the schematics version B1, dated 2019-2-21 (with a different SD card switch circuit).

You have uploaded in this post version A1, dated 2017-12-22.

The development board we just bought through Farnell contains the new silicon (I hope) on an old pcb ???

Can you please double check & clarify what the latest development board, schematics & pcb versions are?

Best regards,

Johan

0 Kudos
Reply
4,446 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

The latest version is B1. What you got is an old version, A1 board with A0 chip. I don't think it could be a A1.

jingpan_0-1652062391625.png

 

Please refer to the errata for their different.

https://www.nxp.com.cn/docs/en/errata/IMXRT1050CE.pdf

 

Regards,

Jing

 

0 Kudos
Reply
4,537 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @trailerman ,

This is A1 schematic.

 

Regards,

Jing

0 Kudos
Reply
4,535 Views
trailerman
Contributor I

Hi Jing,

With regards to the numbers on the board?

What does each of them mean?

 

 

0 Kudos
Reply
4,527 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @trailerman ,

Please see the revision history table in schematic head.

jingpan_0-1650956650813.png

Besides that, the chip is changed from MIMXRT1052DVL6A to MIMXRT1052DVL6B.

 

Regards,

Jing

 

0 Kudos
Reply
3,522 Views
Kaveri
Contributor I

Hi Jing,

 Can you share the layout of this schematic..

Thank you.

0 Kudos
Reply