SDK that supports TWR-SER module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK that supports TWR-SER module

1,293 Views
nickwallis
Senior Contributor I

Hi,

I'm looking to download an SDK that supports the TWR-SER module (particularly the ethernet interface on that module) but am struggling, please can you help?

If it matters, the host board in the tower system is a K64F120M

thanks

-Nick

0 Kudos
Reply
2 Replies

1,282 Views
EdwinHz
NXP TechSupport
NXP TechSupport

I believe this TWR module itself might not be fully supported by our current SDKs. I checked the KSDK as well but found nothing either.

However, you should be able to import the MK64 ethernet drivers and use them without problems on your TWR module.

 

Regards,

Edwin.

0 Kudos
Reply

1,040 Views
fshah30
Contributor II

Hi,

I am using the same PHI KSZ8041NL on my prototype with MK64. The FRDM-K64 board uses KSZ8081 PHY. Please advise how can I import the drivers from SDK to use for KSZ8041NL PHY?

Thank you,

FS

0 Kudos
Reply