QN902X support in MCUxpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QN902X support in MCUxpresso

979 Views
michelkuenemann
Contributor III

Hi NXP,

I plan to use a QN9020 in a new design and I have two questions:

1 - is this device recommended for new designs ? - if NOT, which device does NXP recommend ?

2 - where can I find the MCUxpresso SDK for this device ?

Thanks a lot

Michel Kuenemann

0 Kudos
Reply
3 Replies

830 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Well there is the newer QN device - QN09080

And also in the Kinetis W range, some devices have Bluetooth and MCUXpresso SDKs available 

For more info on supported devices check the mcuxpresso.nxp.com website for downloadable SDKs, plus the MCUXpresso Supported Devices Table 

Regards,

MCUXpresso IDE Support

0 Kudos
Reply

830 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Sorry, there are no plans to support QN9020 in the MCUXpresso environment.

From a quick glance at the product page (QN902x|NXP ) it appears that you will need a copy of IAR or Kei tools, and the QN team provide a product specific SDK (i.e. not an MCUXpresso SDK).

Regards,

MCUXpresso IDE Support

0 Kudos
Reply

830 Views
michelkuenemann
Contributor III

Thanks for prompt reply.

Does NXP provide another BLE SOC which IS supported by MCUXpresso ?

Michel

0 Kudos
Reply