QN902X support in MCUxpresso

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QN902X support in MCUxpresso

1,776件の閲覧回数
michelkuenemann
Contributor III

Hi NXP,

I plan to use a QN9020 in a new design and I have two questions:

1 - is this device recommended for new designs ? - if NOT, which device does NXP recommend ?

2 - where can I find the MCUxpresso SDK for this device ?

Thanks a lot

Michel Kuenemann

0 件の賞賛
返信
3 返答(返信)

1,627件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Well there is the newer QN device - QN09080

And also in the Kinetis W range, some devices have Bluetooth and MCUXpresso SDKs available 

For more info on supported devices check the mcuxpresso.nxp.com website for downloadable SDKs, plus the MCUXpresso Supported Devices Table 

Regards,

MCUXpresso IDE Support

0 件の賞賛
返信

1,627件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Sorry, there are no plans to support QN9020 in the MCUXpresso environment.

From a quick glance at the product page (QN902x|NXP ) it appears that you will need a copy of IAR or Kei tools, and the QN team provide a product specific SDK (i.e. not an MCUXpresso SDK).

Regards,

MCUXpresso IDE Support

0 件の賞賛
返信

1,627件の閲覧回数
michelkuenemann
Contributor III

Thanks for prompt reply.

Does NXP provide another BLE SOC which IS supported by MCUXpresso ?

Michel

0 件の賞賛
返信