你好,我在使用PN5190开发板,用MCUXpresso IDE(版本 v11.8.0)执行Debug时遇到localhost连接超时问题。
我用的开发板主控是MK82,我用的SDK是“NxpNfcCockpit_VCOM_UcBalFW_v03.10.00”。
导入这个SDK后,使用GUI Flash tool可以下载固件,选择“phNncBootloader”和“phUcBal_Secondary”这两个项目可以执行Debug,但选择“Nfcrdlib_SimplifiedAPI_EMVCo_Secondary”项目就会出现连接超时,错误信息如下:
请问要如何解决这个问题呢?
Hello, I tried to run "J-Link GDB Server.exe", change the port as same as the IDE setting and connect, and then the Debug is works fine.
Hello @Fanfei
I truly apologize for the delay. It is good to know that the debug is now working fine! Please let us know if anything else is required.
Regards,
Eduardo.