PEMICRO USB Multilink Universal FX not shown in Debug Config

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PEMICRO USB Multilink Universal FX not shown in Debug Config

1,338 次查看
bitjockey
Contributor II

Hello,

I have been using two different PEMICRO Multilink Universal FX debuggers in both KDS 3.2.0 and MCUXpresso  v11.1.0 3209 and v11.0.1 2563. Not sure what happened, but when I go to the debug configurations screen and select the correct configuration for the GDB PEMICRO Interface Debugging, and then go to the debugger tab where the Revision should be with the device serial number is  blank and hitting refresh does nothing. No matter which IDE I am running. I can't even see them when I use the PEMICRO update utility it shows as non connected. My Segger JLink EDU works, (Connected it just to test) I can use all three of these on another computer, (my personal one) without issue. I have reloaded the latest PEMICRO drivers and multilink software. Even reloaded, KDS v3.2.0. No change. Just wondering if anyone else has ever experienced this and if so, what the fix is?

Thanks

0 项奖励
回复
1 回复

1,261 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Brian,

 

I recommend you to ask your question with the proper PEmicro support in order to have a more suitable support of this debugger.

 

http://www.pemicro.com/support/index.cfm

 

Best regards,

Felipe

0 项奖励
回复