Background: Previously using 10.0.0 with Arm 2017 q1 cross compiler for K64F target.
Just installed v10.1.1 and imported my existing projects.
When I try to build, I get:
Cannot run program "make": Launching failed
Error: Program "make" not found in PATH
In the project properties C/C++ build -> Tool Chain Editor I see "Current Toolchain: Cross GCC" (correct).
In the Tool Chain Editor I also see the "orphaned configuration" error below.

The option "Tools Paths" below Tool Chain Editor is missing (this is were I set the path to the GCC cross compiler in v10.0.0; see image from 10.0.0 below):

How to I configure v10.1.1 to use the external cross-compiler as I used in v10.0.0 so I can get some work done?
Thanks! Best Regards, Dave
PS: To add aggravation, trying 10.1.1 has corrupted the environment/project, so now trying to build the project under 10.0.0 gets the following NullPointerException (very nice):