Open Installed SDKs window?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Open Installed SDKs window?

Jump to solution
1,475 Views
curtis_hendrix
Contributor I

I closed the "Installed SDKs" window, and now I can't figure out to reopen it.  How can I reopen the "Installed SDKs" window?

0 Kudos
Reply
1 Solution
1,379 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Simplest way is probably to use the "Quick Access" box (normally in the top right of the IDE window) and start to enter "Installed SDKs", then click on the view when the appropriate entry appears as you type ....

pastedImage_1.png

Otherwise, use the menu :

  • Window -> Show View -> Other -> MCUXpresso IDE -> Installed SDKs

Regards,

MCUXpresso IDE Support

View solution in original post

1 Reply
1,380 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Simplest way is probably to use the "Quick Access" box (normally in the top right of the IDE window) and start to enter "Installed SDKs", then click on the view when the appropriate entry appears as you type ....

pastedImage_1.png

Otherwise, use the menu :

  • Window -> Show View -> Other -> MCUXpresso IDE -> Installed SDKs

Regards,

MCUXpresso IDE Support

An error has occurred when reading existing sub-variable "Language_PG_Configuration"; see cause exception! The type of the containing value was: extended_hash+string (lithium.coreapi.webui.template.models.NamedValueByNameTemplateModel wrapped into f.e.b.StringModel) ---- FTL stack trace ("~" means nesting-related): - Failed at: #assign redirect_lingo_page_url = web... [in template "language_macro_header.ftl" at line 173, column 1] - Reached through: #include "language_macro_header.ftl" [in template "Language_translator_Dashboard" at line 3, column 1] ----