OM13098 Can program over segger but not Link2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OM13098 Can program over segger but not Link2

2,268件の閲覧回数
whinis
Contributor I

I am having an odd issue on my OM13098. After the first programming with the RNG example I am unable to use MCUXpresso to program the board again over Link2. Link2 appears active, I can put it in DFU mode and program it with CMSIS-DAP using LPCScrypt. I can also access the UART over its VCOMM and have confirmed that UART is working as I can put the board into ISP0 mode and wipe the ROM.

I can also confirm SWD is working as using a Segger JLink on P1 allows me to use MCUXpresso to write the LPC54628.

Using Link2 gives me this error

Unable to open probe index 1.
Error: Probe not open

Also D10 keeps blinking.

0 件の賞賛
返信
12 返答(返信)

2,225件の閲覧回数
ErichStyger
Specialist I

Have you re-programmed it with LPCscrypt back to a CMSIS-DAP probe and the jumper JP1 removed?

0 件の賞賛
返信

2,215件の閲覧回数
whinis
Contributor I

I did, it was one of the first things I tried without success

0 件の賞賛
返信

2,160件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

How about program  it with LPCscrypt   to a jlink probe ?

If all can't work, maybe the debugger on your board broken.

 

BR

Alice

0 件の賞賛
返信

2,151件の閲覧回数
whinis
Contributor I

So previously I had no issue programming it atleast in debug mode, now that is not the case after having programmed a few times using my jlink. It enumerates

Device Description       : LPC based USB device
Device Path              : \\?\usb#vid_1fc9&pid_000c#abcd#{a5dcbf10-6530-11d2-901f-00c04fb951ed}
Device ID                : USB\VID_1FC9&PID_000C\ABCD
Hardware IDs             : USB\VID_1FC9&PID_000C&REV_0100 USB\VID_1FC9&PID_000C


However my usb tester says its broken in some way

    ---------------------- Device Descriptor ----------------------
bLength                  : 0x12 (18 bytes)
bDescriptorType          : 0x01 (Device Descriptor)
bcdUSB                   : 0x200 (USB Version 2.00)
bDeviceClass             : 0x00 (defined by the interface descriptors)
bDeviceSubClass          : 0x00
bDeviceProtocol          : 0x00
bMaxPacketSize0          : 0x40 (64 bytes)
idVendor                 : 0x1FC9 (NXP Semiconductors)
idProduct                : 0x000C
bcdDevice                : 0x0100
iManufacturer            : 0x01 (String Descriptor 1)
 *!*ERROR  String descriptor not found
iProduct                 : 0x02 (String Descriptor 2)
 *!*ERROR  String descriptor not found
iSerialNumber            : 0x03 (String Descriptor 3)
 *!*ERROR  String descriptor not found
bNumConfigurations       : 0x01 (1 Configuration)
Data (HexDump)           : 12 01 00 02 00 00 00 40 C9 1F 0C 00 00 01 01 02   .......@........
                           03 01                                             ..

ConfigDescriptor 1 Error : ERROR_OPERATION_ABORT

 Attempting to use the scripts

LPCScrypt - J-Link firmware programming script v2.0.0 June 2018.

Connect an LPC-Link2 or LPCXpresso V2/V3 Board via USB then press Space.

Press any key to continue . . .

Nothing to boot
Boot Failed:
Ensure One Debug Probe is configured to DFU-Boot and connected via USB.
- For LPC-Link2: remove link JP1 (nearest USB) and power cycle
- For LPCXpresso V2/V3: make DFU link and power cycle

Press any key to continue . . .

 

using DFU

 

C:\nxp\LPCScrypt_2.0.0_831\bin>dfu-util -D C:\nxp\LPCScrypt_2.0.0_831\probe_firmware\LPCLink2\Firmware_JLink_LPC-Link2_20160923.bin
dfu-util 0.8

Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.
Copyright 2010-2014 Tormod Volden and Stefan Schmidt
This program is Free Software and has ABSOLUTELY NO WARRANTY
Please report bugs to dfu-util@lists.gnumonks.org

Invalid DFU suffix signature
A valid DFU suffix will be required in a future dfu-util release!!!
Opening DFU capable USB device...
ID 1fc9:000c
Run-time device DFU version 0100
Claiming USB DFU Runtime Interface...
Determining device status: state = dfuIDLE, status = 0
WARNING: Runtime device already in DFU state ?!?
Claiming USB DFU Interface...
Setting Alternate Setting #0 ...
Determining device status: state = dfuIDLE, status = 0
dfuIDLE, continuing
DFU mode device DFU version 0100
Device returned transfer size 2048
Copying data from PC to DFU device
Download [ ] 0% 0 bytesError during download get_status

0 件の賞賛
返信

2,144件の閲覧回数
whinis
Contributor I

Small update, after unplugging and replugging 5-10 times I got it to flash to jlink and that worked flawlessly then. However reflashing to CMSIS-DAP continues to not work.

0 件の賞賛
返信

2,133件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

How about change to  another PC to test ?

 

0 件の賞賛
返信

2,021件の閲覧回数
whinis
Contributor I

Sorry been busy with life and I don't seem to get emailed from these threads even though its checked. Will need to debug that at another time.

Using another PC did not work and now even using a JLink has stopped working. I  can connect to the debug header and appear to have a connection as the JLink shows voltage. However I cannot connect to the core. I can still flash over USB MSC however I can no longer debug.

0 件の賞賛
返信

2,246件の閲覧回数
whinis
Contributor I

Thought I replied to this earlier, neither deleting the launch file nor starting a new workspace fixed the issue.

0 件の賞賛
返信

2,229件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

OK, thanks for your sharing.

0 件の賞賛
返信

2,173件の閲覧回数
whinis
Contributor I

Is there anything else for my to try or is my board broken in some way ?

0 件の賞賛
返信

2,256件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello whinis,

How about change to a new workspace, open a new project, then click the "Debug" button under "Quickstart Panel" view :

Alice_Yang_0-1618474604225.png

 

 

BR

Alice

0 件の賞賛
返信

2,261件の閲覧回数
ErichStyger
Specialist I

have you tried deleting the .launch file for the LPC-Link2 already and create a new & fresh one?

0 件の賞賛
返信