No compatible probes available. But they are.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No compatible probes available. But they are.

862 Views
alexeym
Contributor III

Just downloaded MCUXpresso v10.1.0 and now I cant list any probes. however if I connect to redlink server over telnet or start it with /redlinkserv --commandline argument PROBELIST command works fine and shows my LPC-LINK2. I tried to debug this problem with debug messages in MCUXpresso IDE but the only messages I see is:

[Started server]
[Closed]
[Closed]

Tags (1)
0 Kudos
1 Reply

664 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Can you confirm what OS (including version) you are running the IDE on? And also whether this is a real machine or a VM ?

Is your LPC-Link2 using firmware pre-programmed into its onboard flash, or are you relying on the IDE to soft load the firmware?

If you are softloading, does manually boot the probe help at all (as described in the MCUXpresso IDE v10.1.0 User Guide, section 16.9, "Using and troubleshooting LPC-Link2"). It might also be worth programming the firmware into the flash if you are softloading, using LPCScrypt.

Regards,

MCUXpresso IDE Support.

0 Kudos