No available probe with MCUXpresso IDE and LPCXpresso 1769 board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

No available probe with MCUXpresso IDE and LPCXpresso 1769 board

1,214 次查看
madcitymann
Contributor I

First use of LPCXpresso 1769 board and MCUXpresso IDE. I'm not getting any COM devices showing up in device manager. I do get a 'MBED microcontroller USB Device' under Disk Drives. When I reset the board, it looks like it's running a defualt program that blinks the Green LED once per second. I do have other development boards that do show up under 'Ports (COM & LPT), when plugged in. Am I missing a driver?

0 项奖励
回复
3 回复数

1,100 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Timothy Holzmann,

How about  install MBED serial driver? 

Windows serial configuration - Handbook | Mbed  

Hope it helps,


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,100 次查看
madcitymann
Contributor I

Yes, I tried that and it works. I now want to update the debug firmware. I

haven't found definitive instructions on how to update the firmware on my

board - an LPCXspresso 1769 Rev D. The board itself has a Rev D2, there is

a schematic available for a Rev D and Rev D1. The Rev D1 is different, it

looks like the Rev D matches the Rev D2 hardware - can you confirm?

Thanks

Tim

0 项奖励
回复

1,100 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Tim,

"

 how to update the firmware on my

board - an LPCXspresso 1769 Rev D. 

"

-> If your board is Rev D, please refer to the Rev D schematic. 

And how to update the debug firmware please refer to the below thread:

LPCXpresso LPC1769 (OM13085) Can't find debug Probe  

Brendon Slade said: 

"You can find that firmware by searching for "lpc11u35 debug firmware" or directly at this link: https://www.nxp.com/webapp/sps/download/license.jsp?colCode=LPC11Uxx-Debug-Probe-VCOM&fsrch=1&sr=1&p...=

This package includes a driver for the VCOM function, plus the new debug probe firmware and instructions to install. Updating the firmware is easy - hold down reset while powering the board and you will see a device called CRP_DISABLD appear in your file manager. Delete the file there called firmware.bin, then drag and drop the file with the same name from the package you downloaded. Re-power the board and away you go!"

Hope it helps,


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复