NO PWM in LPC1788 LPCOPEN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NO PWM in LPC1788 LPCOPEN

1,419 Views
Simon0527
Contributor I

hey,guys:

I have a lpc1778 board , and now i need a lpcopen pwm driver . but i can not find it in the 2.10.zip ,

who can help me and provide a pwm module drivers of Lpc177x_8x for me .

Simon.

0 Kudos
Reply
3 Replies

1,408 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Simon0527,

It seems there is no driver, while this is AN10898, it is a demo about BLDC motor control with LPC1700,

you can download and refer to it:

https://www.nxp.com.cn/docs/en/application-note/AN10898.zip 

 

BR

Alice

0 Kudos
Reply

1,383 Views
Simon0527
Contributor I

Thanks for your reply:

   but  you know, I want to use  MUXPresso IDE to complete my project , and connect with LPCOPEN .

maybe official did not support pwm lpcopen in MUXPresso IDE yet , so I just want to know if have the 

driver like this : https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-Pwm-Driver/m-p/583807

Simon0527_0-1633743664533.png

his zip has already disappeared . so if have the new one?

by Simon.

0 Kudos
Reply

1,378 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Simon,

Sorry I also haven't find this.

 

BR

Alice

0 Kudos
Reply