As per the KL26/KL16 series reference Manual, there are no IRQ handlers for PORT B and PORT E.
But PORT A is available (irq 30) and Port C and Port D are available on One ISR (irq 31).
I want to have PORT B and PORT E also to be used as Interrupt pins but they are unavailable to generate an ISFR bit set when they are configured as (PCR Reg using PORT_SetPinInterruptConfig()).
Is this to say there are no Hardware module present internal to chip responsible for these ports Interrupt. ( ISFR are available but they are going to be useless) there is no hardware detection for when these port pins are asserted?
Also, is there a way to configure them at all on KL chips? As also software interrupts are also not available on KL chips/
Please Advise.
Thank you
Abhi