Missing peripherals tools in MCUXpresso IDEv11.6.0 in project with SDK_2_11_0_MKE06Z128xxx4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Missing peripherals tools in MCUXpresso IDEv11.6.0 in project with SDK_2_11_0_MKE06Z128xxx4

Jump to solution
909 Views
CMH1
Contributor II

Hello All,
Using MCUxpresso 11.6.0 and SDK MKE06Z128xxx4 Version 2.11.0 for processor MKE06Z128VLD4. Not sure if it's something I've done but several peripherals are missing from the peripherals tool. The drivers are available when setting up a new project, source and header files are created in the project. For example, MSCAN/Flexcan, ADC, RTC are not show. See the attached screen shots showing the peripheral config page and the Manage SDK window. Any ideas?

0 Kudos
Reply
1 Solution
899 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi CMH1 

For the moment  MSCAN/Flexcan, ADC, RTC are not implemented in peripheral tool in KE128. I will escalate it as feature request to config tool team.  Please use SDK component for these peripheral.

Thanks for bringing the problem to our attention.

Have a nice day,

Jun Zhang

View solution in original post

0 Kudos
Reply
2 Replies
895 Views
CMH1
Contributor II

Thank you for the help. 

0 Kudos
Reply
900 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi CMH1 

For the moment  MSCAN/Flexcan, ADC, RTC are not implemented in peripheral tool in KE128. I will escalate it as feature request to config tool team.  Please use SDK component for these peripheral.

Thanks for bringing the problem to our attention.

Have a nice day,

Jun Zhang

0 Kudos
Reply