Memory view

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Memory view

2,786 次查看
carstenhoffmann
Contributor I

Hi,

I am using MCUXpresso and I have a beginners question.

Everytime I start a new debug session (with terminate, build, debug), all my memory monitors are removed.

I have to add them by hand for each new session.

Is there any way to keep the memory monitors?

Thanks for help,

Carsten

0 项奖励
回复
1 回复

2,555 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

Sorry, no. There is no way currently of automatically re-populating the Memory View from previous debug sessions.

Couple of things that may help to a degree. If you are viewing memory at the base addresses of RAM or Flash regions defined for the project, then these will be listed for quick selection towards the bottom of the list of peripherals in the Peripherals View. In addition the + button in the Memory View will keep a list of previously viewed memory locations in the drop down for the duration of the IDE current session, which can save having to type the address in again.

Regards,

MCUXpresso IDE Support

0 项奖励
回复