MIMXRT1064 flash tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1064 flash tool

1,089 Views
max_yang1
Contributor III

Is there a standalone flash tool that can program the MIMXRT1064 internal flash outside of IDE? 

Thanks,

 

Max

0 Kudos
Reply
5 Replies

1,026 Views
liborukropec
NXP Employee
NXP Employee

Hi Max,

SEC tool does not use JTAG, SEC tools talks directly with the Serial Downloader implemented in the device ROM. I do not know what HW you use - your proprietary or still NXP EVK?

 

If proprietary then you need to look to the Reference Manual (if link works, it should be accessible from here https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/i-mx-rt-crossover-...)

then look to the chapter 9 System Boot - in short the device must start ISP - using either GPIO pins or fuses and then communicate with ROM via USB1 or LPUART1, see here

 

liborukropec_0-1706548275564.png

 

More details can be found in the mentioned RM. IMHO the problem less should be the serial communication with proper USB to serial converter with proper voltage levels.

 

Regards,

Libor

0 Kudos
Reply

1,021 Views
max_yang1
Contributor III

Libor,

We can refer to NXP EVK for this conversation (should be similar), however we may not have a physical access to USB1/UART1/SPI for that purpose. The only thing available for that is JTAG for sure. In that case what kind tool available for that?

Max

0 Kudos
Reply

1,001 Views
liborukropec
NXP Employee
NXP Employee

Hi Max,

I'm afraid I'm aware only about GUI Flash tool inside IDE, and then the stand-alone Secure Provisioning Tool.

Libor

0 Kudos
Reply

1,066 Views
liborukropec
NXP Employee
NXP Employee

Hello Max,

there's a Secure Provisioning Tool supporting your use case (MIMXRT1064). See here https://www.nxp.com/mcuxpresso/secure

There's also a community for this tool - here https://community.nxp.com/community/mcuxpresso/mcuxpresso-secure-provisioning-tool

 

Regards,

Libor

0 Kudos
Reply

1,032 Views
max_yang1
Contributor III

Libor,

Thanks for the links.

Saw this on features of the tool

"Support target connectivity via UART, USB-HID, SPI, and I2C serial download modes"

Not sure on the target connections. I have USB/JTAG probe to the processor. Which type does it covered?

Thanks,

Max

0 Kudos
Reply