MIMRT170 lwip TCP/IP server and client example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMRT170 lwip TCP/IP server and client example

1,692件の閲覧回数
gurukiran
Contributor I

Hi,

I need to do client and server program for MIMRT1170-EVKB board using LWIP TCP/IP Stack and freeRTOS.

Please provide the example for TCP client and TCP server program. As ping is working fine. For that I need to add TCP client and TCP server program.

Thank you,

GuruKiran M B

0 件の賞賛
返信
1 返信

1,651件の閲覧回数
gurukiran
Contributor I

Hi Nxp,

From the nxp community Forum, we got info on how the socket creation works, things to configure for tcp-client.
From that idea , we have coded for both tcp-client and tcp-server and it will be helpful for others to refer while implementing the same.

Tcp-client and server implementation include transmitting the data in the packets and receiving the acknowledgement.

A special thanks to my teammates: Har**bleep**ha R and Niranjan for their support while implementing the same.

PFA attached code for the same.

Thanks,

Gurukiran M B

0 件の賞賛
返信