MCUXpresso v11.8 and MCU-Link = SocketException?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso v11.8 and MCU-Link = SocketException?

2,150 Views
arnogir
Senior Contributor II

Hello

 

Unitl now, I used MCUXpresso v11.6 with MCULink Fw=2.263 and all work properly

I installed MCUXpresso v11.8 and updated MCULink to Fw 3.122.

Now in MCUxpresso I get the following message when I try to discover probe by clicking on "Debug":

arnogir_0-1696149847493.png

 

Is somebody can help me to found were come from the problem?

0 Kudos
Reply
8 Replies

1,497 Views
arnogir
Senior Contributor II

Hello,

 

I'm always unable to use my MCU-LINK with newer version of MCUXpresso

 

I Just tried with last v11.9 without success:

arnogir_0-1708253165339.png

 

I updated MCU-link firmware to the v3.133 (try with both "CMSIS and JLINK)...

Are they a way to make run with v11.9 (I read this version will automaticcaly upgrade firmware..?)

So the only solution is to stay on v11.6

 

Note: now on MCU-link NXP web page, it only proposed the v2.263 driver...?

 

Thank

0 Kudos
Reply

1,989 Views
arnogir
Senior Contributor II

Hello,

Sorry for the late.

I tried with new workspace, With MCU-link alone or connected to the end board, uninstall/re install MCUXpresso without success.

Why pass from MCUlink FW 2.x to 3.x, because it is indicated the MCUXpresso 11.7 or upper are only compatible with FW 3.x...

Regards

0 Kudos
Reply

1,976 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @arnogir,

Could you please tell us which OS are you using? Additionally, could you please try testing the behavior using another computer?

Start mcuxpresso and create basic project with wizard.

Have you tried using an example? Does this basic project already contain a Launch Configuration file? If so, could you please try deleting the Launch file, before going to Debug?

Also, have you tried debugging with another board to see if that debug probe is being detected in the Debug Probe Discovery? Could you please try debugging with the FW 2.x?

Best regards, Raul.

0 Kudos
Reply

2,096 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @arnogir,

Just for double check, do you remove the jumper after the update?

We tested the MCUXpresso IDE v11.8.0 with the v3.122 FW of MCU-Link. On our side we could successfully discovered the MCU-Link board alone and after connecting with an LPCXpresso55S69-EVK.

Could you please describe your steps to try to replicate your issue on our side?

Best regards, Raul.

0 Kudos
Reply

2,091 Views
arnogir
Senior Contributor II

Hello.

 

Yes j3 was removed.

I did like done with v11.6:

Install mcuxpresso

Flash mculink fw

Start mcuxpresso and create basic project with wizard.

Compile

Try to link with mculink (debug button)

 

I revert to v11.6/fw v2.xxx work nice.

Retry to upgrade fw 3.122 and with mcuxpresso 11.8=crash (see my first message for screenshots)

My be can I activate a log or trace to give you some additionnel information?

 

0 Kudos
Reply

2,088 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @arnogir,

Could you please tell us which script are you running?

RaulRomero_0-1696284290936.png

[MCU-LINK -> scripts]

Could you please try it with program_CMSIS?

Best regards, Raul.

0 Kudos
Reply

2,074 Views
arnogir
Senior Contributor II

Hello

 

I always use the cmsis

 

0 Kudos
Reply

2,052 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @arnogir,

Could you please try in a new workspace? Are you connecting the MCU-Link with another board or just by itself? Finally, could you please try reinstalling the MCUXpresso IDE v11.8.0?

Also, is there any special reason to update to the newest MCU-Link Firmware? You could still use the old version in the newest MCUXpresso IDE, if there is not a special requirement to update the FW.

Best regards, Raul.

0 Kudos
Reply