MCUXpresso v11.2.0 Create New C/C++ Project Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso v11.2.0 Create New C/C++ Project Problem

1,146 Views
jgriggs
Contributor I

Hello,

I recently installed MCUXpresso v11.2.0 and created a new v2.8.0 SDK build for the MKE14F512VLL16 MCU and installed it into the IDE. I then proceeded to create a new project by clicking Create a new MCUXpresso IDE C/C++ project in the IDE.

I selected my appropriate device as follows:

cature1.PNG

I then selected all of the device drivers for my baremetal project:

cature2.PNG

And finally the problem showed up, I'm unable to set a library type or Floating point type for my processor. The drop down menus are blank.

cature3.PNG

I went through this same exercise using SDK v2.7.0 and I had the same problem so it seems like the problem is MCUXpresso related.  Note that this process worked previously with MCUXpresso v11.1.1 and SDK v2.7.0.

Any suggestions on how to fix this?

Regards,

Jesse

Labels (1)
3 Replies

1,035 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Jesse,

I hope you are doing great.

I am checking the issue that you are facing. I will get back to you as soon as possible.

I recommend working with the previous MCUxpresso version.

Regards,

Mario

0 Kudos

1,035 Views
jgriggs
Contributor I

Hi Mario,

Thanks for looking into this for me. I can supply any needed files or more screen shots if needed to help troubleshoot.

Regards,

Jesse

0 Kudos

1,035 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Thank you for your report. We logged a ticket internally to track the problem. We're planning to have it fixed in the next release.

Greetings,
MCUXpresso IDE Support