MCUXpresso v11.1.1 has exception with MIMXRT1064-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso v11.1.1 has exception with MIMXRT1064-EVK

911 Views
serbul
Contributor I

Hello,

I'm using MCUXpresso IDE v11.1.1 [Build 3241] [2020-03-02] under Ubuntu 16.04 with MIMXRT1064-EVK. I see exception in redlinkserv process during start debug session (full dump is attached):

........

*** Error in `/usr/local/mcuxpressoide-11.1.1_3241/ide/plugins/com.nxp.mcuxpresso.tools.bin.linux_11.1.0.202002241259/binaries/redlinkserv': malloc(): memory corruption: 0x00007fb8440e2ee0 ***
======= Backtrace: =========
/lib/x86_64-linux-gnu/libc.so.6(+0x777e5)[0x7fb8525917e5]
/lib/x86_64-linux-gnu/libc.so.6(+0x8213e)[0x7fb85259c13e]
/lib/x86_64-linux-gnu/libc.so.6(__libc_malloc+0x54)[0x7fb85259e184]
/usr/lib/x86_64-linux-gnu/libstdc++.so.6(_Znwm+0x18)[0x7fb852e981e8]
/usr/local/mcuxpressoide-11.1.1_3241/ide/plugins/com.nxp.mcuxpresso.tools.bin.linux_11.1.0.202002241259/binaries/redlinkserv[0x40a70e]
/usr/local/mcuxpressoide-11.1.1_3241/ide/plugins/com.nxp.mcuxpresso.tools.bin.linux_11.1.0.202002241259/binaries/redlinkserv[0x40cba4]
/usr/local/mcuxpressoide-11.1.1_3241/ide/plugins/com.nxp.mcuxpresso.tools.bin.linux_11.1.0.202002241259/binaries/redlinkserv[0x41c72c]
/usr/local/mcuxpressoide-11.1.1_3241/ide/plugins/com.nxp.mcuxpresso.tools.bin.linux_11.1.0.202002241259/binaries/redlinkserv[0x42898c]
/usr/local/mcuxpressoide-11.1.1_3241/ide/plugins/com.nxp.mcuxpresso.tools.bin.linux_11.1.0.202002241259/binaries/redlinkserv[0x428f24]
/usr/local/mcuxpressoide-11.1.1_3241/ide/plugins/com.nxp.mcuxpresso.tools.bin.linux_11.1.0.202002241259/binaries/redlinkserv[0x4158ad]
/usr/local/mcuxpressoide-11.1.1_3241/ide/plugins/com.nxp.mcuxpresso.tools.bin.linux_11.1.0.202002241259/binaries/redlinkserv[0x4098d6]
/lib/x86_64-linux-gnu/libpthread.so.0(+0x76ba)[0x7fb8531986ba]
/lib/x86_64-linux-gnu/libc.so.6(clone+0x6d)[0x7fb85262141d]

........

I cannot connect to DAPLink CMSIS-DAP debugger under Ubuntu 16.04, but it works correctly from Windows.

I will be grateful for any help.

BR

Sergey

0 Kudos
Reply
1 Reply

857 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello Sergey,

Hope you are doing well.

I was not able to reproduce this error on my end. I am using Ubuntu 16.04, MCUXpresso IDE 11.1.1 and SDK 2.7.0 for the iMXRT1064-EVK.

Are you able to work with other microcontrollers? To discard that there was any issue installing MCUXpresso IDE?

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos
Reply