MCUXpresso sh.exe crash cygwin error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCUXpresso sh.exe crash cygwin error

跳至解决方案
2,199 次查看
ivaylomanushev
Contributor II

Hello All,

   I am having an issue every time I build my project I get an error that I shouldn't:

m.AllocationBase 0x0, m.BaseAddress 0x71110000, m.RegionSize 0x4C0000, m.State 0x10000
C:\nxp\MCUXpressoIDE_10.0.0_344\ide\msys\bin\sh.exe: *** Couldn't reserve space for cygwin's heap (0x71110000 <0x2930000>) in child, Win32 error 0

Now if I keep pressing the build button the project would compile after the 2nd or 3rd sometimes 4th consecutive build. 

Sometimes I would get a windows error that sh.exe has crashed with Fault Module Name: msys-1.0.dll

Any help in solving this issue would be appreciated!

Thanks,

Ivaylo

0 项奖励
回复
1 解答
1,893 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

Please see section 14.9, "Make fails with Virtual Alloc pointer is null error", of the MCUXpresso IDE v10.0.0 User Guide.

Regards,

MCUXpresso IDE Support

在原帖中查看解决方案

2 回复数
1,894 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

Please see section 14.9, "Make fails with Virtual Alloc pointer is null error", of the MCUXpresso IDE v10.0.0 User Guide.

Regards,

MCUXpresso IDE Support

1,892 次查看
ivaylomanushev
Contributor II

Thanks for the info that worked like a charm!

0 项奖励
回复