MCUXpresso hangs on startup after laptop crash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCUXpresso hangs on startup after laptop crash

跳至解决方案
913 次查看
hfuhruhurr
Contributor III

Hi there,

I'm using MXUXpresso 11.5 on an older project with a LPC1768 process (actually, it's a project with 3 subprojects).

My computer crashed today while MCUX was open but idling. After restarting the computer, MCUXpresso starts up, shows the IDE (full screen, code is displayed, even with correct highlighting of compiler switches) but then freezes.

Is there any condition which has to be removed (clean lock files or folders, workspace ...) that helps?

Best regards

Rainer

0 项奖励
回复
1 解答
905 次查看
hfuhruhurr
Contributor III

I managed to revive it by replacing the workspace folder contents with the ones from a recent backup.

I'd still be interested in a solution (or at least background information on the problem).

在原帖中查看解决方案

0 项奖励
回复
3 回复数
844 次查看
hfuhruhurr
Contributor III

I stated: The IDE shows up, displays code but then freezes.

I can't clean, refresh or build anything.

I don't think this will be resolved, here, let's just forget about it.

Best regards,

Rainer

0 项奖励
回复
906 次查看
hfuhruhurr
Contributor III

I managed to revive it by replacing the workspace folder contents with the ones from a recent backup.

I'd still be interested in a solution (or at least background information on the problem).

0 项奖励
回复
888 次查看
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, this is difficult to replay, is not really an issue from the IDE, it was a problem for the bad shutdown. Before replacing the workspace did you try to clean, refresh and build again?

Best regards,
Pavel

0 项奖励
回复