MCUXpresso can't access the lpc11u68 after the first time of debugging.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso can't access the lpc11u68 after the first time of debugging.

Jump to solution
1,217 Views
wangwenyu
Contributor II

I use MCUXpresso to connect my target board through a MCU-Link pro. The target board is a simple system on which a LPC11U68 connects a NTAG plus chip through IIC. The ROM driver is used.

It works properly at the first time when I debug this board. But, after I repower the target board, the MCUXpresso never connects with the target board again. This problem continuously occured on my 5 boards. The first time always works. Then the MCUXpresso never connects the target again. 

wangwenyu_0-1676965401284.png

It is highly appreciated if some body help me.

I have struggled for 4 days. No clue is found. 

0 Kudos
1 Solution
1,194 Views
lpcxpresso_supp
NXP Employee
NXP Employee

I'm tempted to say that Code Read Protection was accidentally enabled on your MCUs. Please take a look in the User Manual:

lpcxpresso_supp_0-1676989420964.png

Also, a quick inspection of the projects you attached, illustrate that address 0x0000_02FC is populated with actual implementation of "HW_setup_Board_for_use_with_NTAG" function, meaning that CRP is affected.

lpcxpresso_supp_1-1676989568844.png

I suggest you create a sample project using the NPW from the IDE and inspect "crp.c and "crp.h".

lpcxpresso_supp_2-1676989750248.png

Moreover, please take a look at the generated linker script.

lpcxpresso_supp_3-1676989811156.png

There's also an application note that might be useful: https://www.nxp.com/docs/en/application-note/AN10968.pdf

Regards,
MCUXpresso IDE Support

 

 

 

View solution in original post

6 Replies
1,195 Views
lpcxpresso_supp
NXP Employee
NXP Employee

I'm tempted to say that Code Read Protection was accidentally enabled on your MCUs. Please take a look in the User Manual:

lpcxpresso_supp_0-1676989420964.png

Also, a quick inspection of the projects you attached, illustrate that address 0x0000_02FC is populated with actual implementation of "HW_setup_Board_for_use_with_NTAG" function, meaning that CRP is affected.

lpcxpresso_supp_1-1676989568844.png

I suggest you create a sample project using the NPW from the IDE and inspect "crp.c and "crp.h".

lpcxpresso_supp_2-1676989750248.png

Moreover, please take a look at the generated linker script.

lpcxpresso_supp_3-1676989811156.png

There's also an application note that might be useful: https://www.nxp.com/docs/en/application-note/AN10968.pdf

Regards,
MCUXpresso IDE Support

 

 

 

1,174 Views
wangwenyu
Contributor II

Hi. Not lucky

I used a brand new board (a new MCU) and added the .crp section. But the problem still exists

wangwenyu_0-1676996420969.pngwangwenyu_1-1676996483299.png

 

There is __CRP const unsigned int CRP_WORD = CRP_NO_CRP; in the cr_startup_lpc11u6x.c

 

0 Kudos
1,171 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Obviously... It won't work if you simply add the CRP section now. Your MCUs are most likely locked and debug access is no longer possible because of the previously generated incorrect images. Have you looked in the CRP-related header I suggested? There are comments that mention tools to recover your MCUs.

Regards,
MCUXpresso IDE Support

 

0 Kudos
1,161 Views
wangwenyu
Contributor II

 It is a brand new board. It worked with the simulator at the beginning. I successfully debug this board with a new built image which already NO-CRP at 0x2fc according to your suggestion. (see the image in the last post)

unfortunately, it is locked after I reconnected it.  

I have 4 boards left. 6 Boards are dead.  Hope I can get a clue before I try the next board.

Thank you!

@lpcxpresso_supp 

0 Kudos
1,165 Views
wangwenyu
Contributor II

I forgot to tell that it is a brand new board. It worked with the simulator at the beginning. I successfully debug this board with a new built image which already no-crp at 0x2fc according to your suggestion. 

unfortunately, it is locked after I reconnected it. 


There isn't UART circuit on this board. It isn't possible to recover the board. Flash Magic doesn't support USB for the LPC11U6x.

0 Kudos
1,184 Views
wangwenyu
Contributor II

Thanks. 

I have to enable "Enable automatic placement of code read protection field in image".

wangwenyu_0-1676995012903.png

Then I have:

wangwenyu_1-1676995047468.png

 

Let me try it. Thank you again

 

0 Kudos