MCUXpresso IDE v10.1.1 LinkServer not found

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso IDE v10.1.1 LinkServer not found

Jump to solution
7,446 Views
marianovedovato
Contributor III

Hi everyone!

I've installed MCUXpresso IDE in Linux (Debian but I have seen the same behaviour in Ubuntu).

Following, my problem:

When I want to debug my lpcxpresso 1768/1769 REV B (the same behaviour for REV C and REV D) cannot find the target:

Captura de pantalla de 2018-07-14 08-45-35.png

Some output console:

[Started server]
[Connected on port 3025]
redlink>ProbeList
No probes found
redlink>ProbeList
No probes found
redlink>ProbeList
No probes found
redlink>ProbeList
No probes found
redlink>ProbeStatus
redlink>quit
[Closed]

The project and the workspace are new ones, created from MCUxpresso itself.

-----------------------------------------------------------------------------------------------------------------------------------------------------------

But, if I try to debug with my old installation LPCXpresso v8.2, after the seek for any enabled emulator, I can debug without problems. Picture with LCPXpresso:

Captura de pantalla de 2018-07-14 08-51-02.png

After pressing the button "Search for any...":

Captura de pantalla de 2018-07-14 08-51-10.png

After that, if I use again MCUxpresso I can debug without problems.

All of above are repeat when I disconnect the tool from usb.

My problem is that I can't to migrate to MCUxpresso in these conditions.

Please, any suggest?

BR!

Mariano

Labels (1)
1 Solution
5,189 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Mariano

We have managed to replicate your problem. 

MCUXpresso IDE (and LPCXpresso) uses a background server, the 'link server' to manage debug connections via multiple probes.  It is visible in e.g. 'ps auxw | grep redlinkserv'.  It is this service to which you issued the 'ProbeList' command - which is how the IDE locates the Link1 probe that is part of your LPC1769 board.

The link server comes and goes, but is more persistent in MCUXpresso IDE than in LPCXpresso.  In MCUXpresso it can be terminated using the new 'Clean Up Debug' icon on the toolbar.  It will simply be restarted when needed.

Your LPC1769 board's debug firmware is booted using the 'dfu-util' utility that is part of Debian/Ubuntu.  An unbooted probe can be seen in the output of 'dfu-util -l'.  Once booted 'lsusb' will show a different entry for the probe.  The IDE detects whether the firmware is booted and reboots it if necessary.  We believe that this part of the IDE is working perfectly in your case.

The link server detects only booted probes.  It seems that, in your case, that if the probe is power cycled the IDE reboots the firmware but the link server does not register the new probe (even though it did before the power cycle).

Can you confirm that - when the probe discovery dialogue can not find the probe - you can cancel the discovery; then use the 'Clean Up Debug'; then find that the probe is then discovered properly?

Sincerely

MCUXpresso IDE Support

View solution in original post

5 Replies
5,189 Views
lpcxpresso_supp
NXP Employee
NXP Employee

What is the actual version of Ubuntu that you have seen this issue on?

Is this Ubuntu running natively on your PC, or inside a virtual machine?

Do you see the same behaviour with the current MCUXpresso IDE v10.2 as well?

Can you check if your LPC-Link on your LPCXpresso1769 board appears both before it is booted and after it is booted (using lsusb or similar) ?  [ This FAQ may assist in doing this :  https://community.nxp.com/message/630541 . Although this was written for LPCXpresso IDE, the basic information still applies to MCUXpresso IDE. ]

Regards,

MCUXpresso IDE Support

0 Kudos
Reply
5,189 Views
marianovedovato
Contributor III

Hi support, thank you so much for your reply.

My OS is Debian 9.4 and the Ubuntu that I have seen the same behaviour was 16.04 LTS (or 16.02 I don't remember well). Both cases running natively.

In Ubuntu, I have seen similar behaviour for MCUxpresso 10.2 (I can try in my Debian with 10.2 IDE, I will back soon with the results)

1) Before, and MCUxpresso working fine:
dmesg:

[ 382.838621] usb 1-2: new high-speed USB device number 4 using xhci_hcd
[ 382.978960] usb 1-2: New USB device found, idVendor=0471, idProduct=df55
[ 382.978966] usb 1-2: New USB device strings: Mfr=0, Product=0, SerialNumber=0

lsusb:

Bus 001 Device 005: ID 1fc9:0009 NXP Semiconductors

2) Disconnect LPC1769 from the USB and back to connect (MCUxpresso cant see the target):

dmesg:

[ 1703.260660] usb 1-2: new high-speed USB device number 6 using xhci_hcd
[ 1703.401541] usb 1-2: New USB device found, idVendor=0471, idProduct=df55
[ 1703.401549] usb 1-2: New USB device strings: Mfr=0, Product=0, SerialNumber=0

lsusb:

Bus 001 Device 006: ID 0471:df55 Philips (or NXP) LPCXpresso LPC-Link

3) After back to live with LPCxpresso IDE:

dmesg:

[ 1296.936481] usb 1-2: new high-speed USB device number 5 using xhci_hcd
[ 1297.081270] usb 1-2: New USB device found, idVendor=1fc9, idProduct=0009
[ 1297.081272] usb 1-2: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ 1297.081273] usb 1-2: Product: LPC-Link Probe v1.3
[ 1297.081275] usb 1-2: Manufacturer: Code Red Technologies
[ 1297.081276] usb 1-2: SerialNumber: WIN64HS12

lsusb:

Bus 001 Device 007: ID 1fc9:0009 NXP Semiconductors

I could see that device changed from 6 to 7, and in some probe I have seen this when I use with LPCxpresso, maybe help you:

dmesg:

[ 1296.672755] usb 1-2: reset high-speed USB device number 4 using xhci_hcd
[ 1296.812605] usb 1-2: device firmware changed
[ 1296.812732] usb 1-2: USB disconnect, device number 4
[ 1296.936481] usb 1-2: new high-speed USB device number 5 using xhci_hcd
[ 1297.081270] usb 1-2: New USB device found, idVendor=1fc9, idProduct=0009
[ 1297.081272] usb 1-2: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ 1297.081273] usb 1-2: Product: LPC-Link Probe v1.3
[ 1297.081275] usb 1-2: Manufacturer: Code Red Technologies
[ 1297.081276] usb 1-2: SerialNumber: WIN64HS12

Thank you so much!

Mariano

0 Kudos
Reply
5,190 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Mariano

We have managed to replicate your problem. 

MCUXpresso IDE (and LPCXpresso) uses a background server, the 'link server' to manage debug connections via multiple probes.  It is visible in e.g. 'ps auxw | grep redlinkserv'.  It is this service to which you issued the 'ProbeList' command - which is how the IDE locates the Link1 probe that is part of your LPC1769 board.

The link server comes and goes, but is more persistent in MCUXpresso IDE than in LPCXpresso.  In MCUXpresso it can be terminated using the new 'Clean Up Debug' icon on the toolbar.  It will simply be restarted when needed.

Your LPC1769 board's debug firmware is booted using the 'dfu-util' utility that is part of Debian/Ubuntu.  An unbooted probe can be seen in the output of 'dfu-util -l'.  Once booted 'lsusb' will show a different entry for the probe.  The IDE detects whether the firmware is booted and reboots it if necessary.  We believe that this part of the IDE is working perfectly in your case.

The link server detects only booted probes.  It seems that, in your case, that if the probe is power cycled the IDE reboots the firmware but the link server does not register the new probe (even though it did before the power cycle).

Can you confirm that - when the probe discovery dialogue can not find the probe - you can cancel the discovery; then use the 'Clean Up Debug'; then find that the probe is then discovered properly?

Sincerely

MCUXpresso IDE Support

5,189 Views
marianovedovato
Contributor III

Hi dear support,

I installed 10.2 version (and fixed the "Null pointer" error by enabling "shared file" in the debug configuration).

Later, with the use the 'Clean Up Debug' suggested by you finally I could debug my lpcxpresso LPC1769.

So, thank you so mucho for your appreciate help!

BR

Mariano

0 Kudos
Reply
5,189 Views
marianovedovato
Contributor III

Dear support, thank you so much again for your reply.

I had to upgrade to MCUxpresso v10.2 since the "Clean debug button" didn't appear (or I can't found it) in my older 10.1 version.

And, what now?

When I try to debug my lpc1769 stick, the following message appears:

Captura de pantalla de 2018-07-17 20-17-06.png

pastedImage_3.png

I tried to do a new Workspace, new project but the final result is the same.

I have seen before this error weeks ago, and I remember that the solution was do a downgrade to 10.1 version (note that I am in a kind of infinite loop :smileyhappy:) but the new problems that rised, were regard to a this discussion.

Believe me, my next discussion was going to be the java.lang.NullPointerException.

I will wait for your comments!

BR

Mariano

0 Kudos
Reply