MCUXpresso IDE fail to debug on KW41z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso IDE fail to debug on KW41z

1,497 Views
satsok_n
Contributor III

I recently bought a Freedom KW41Z package with 2 development boards. Even though everything worked perfectly with the first board, when I tried to use the second one I got a debug error.

pastedImage_1.png

Any suggestions?

Tags (1)
0 Kudos
Reply
7 Replies

1,386 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Kostas,

What is the MCUxpresso version that you are working on?

Are you working with the P&E Micro drivers? Could you please erase the launch file and try it again?

Regards,

Mario

0 Kudos
Reply

1,386 Views
satsok_n
Contributor III

Hi Mario

I am working with MCUXpresso IDE v11.0.0 [Build 2516] [2019-06-05]. I tried erasing the launch file but nothing happened. I am using J-Link to debug. It seems that when I debug the with the second dev board It starts with the same S/N of the previous dev board. On the debugging options on the j-link tab I changed the S/N but nothing happened.

0 Kudos
Reply

1,386 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Kostas,

Could you please update the MCUxpresso IDE to v11.1?

Then, could you please erase the memory using the JLink Command? 

Commands: Erase and unlock kinetis

Regards,

Mario

0 Kudos
Reply

1,388 Views
satsok_n
Contributor III

Hi Mario

this is the outcome of:

erase

1.PNG

2.PNG

unlock

3.PNG

and I think the problem is on the serial number

4.PNG

the serial number of second frdm-KW41z is kind of weird. It has established the first KW41Z serial number.

0 Kudos
Reply

1,388 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Kostas,

When you try to enter in debug mode, are you seeing the next message?

pastedImage_1.png

As your terminal log is showing the same message, could you please select the yes option?

Regards,

Mario

0 Kudos
Reply

1,388 Views
satsok_n
Contributor III

Hi Mario

done that but nothing happened. At the end of the terminal I got the message couln't connect to target.

0 Kudos
Reply

1,388 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Kostas,

Unfortunately, your device has been bricked. 

pastedImage_7.png

Could you please submit a warranty request? 

Returns and Warranty Information

Regards,

Mario

0 Kudos
Reply