MCUXpresso IDE can't find my CMSIS-DAP probe.My MCUXpresso IDE version is:MCUXpresso IDE v11.5.1 [Build 7266] [2022-04-13] and running on WINDOWS 10.
but the J-link command can find my CMSIS-DAP probe,thougth it can't download my program.
These two problems bother me for weeks,I can do nothing with my evaluation board an CMSIS-DAP.
Is any solution to finding no compatiable probe problem?
Solved! Go to Solution.
Hello
You said you changed the "JLinkDevices.xml of jlink", how about do not change it, also use the latest J-commander .
About this question “I'm very confused about that why I can download code using J-Flash but failed when use J-commander.”, how about also ask Segger customer support, maybe they know it well.
https://www.segger.com/support/technical-support/
BR
Alice
Hello ,
Is your board custom board? How about have a look at this thread:
BR
Alice
Hi
Alice
I do use a custom board,and it was bought from a third-party vender.The vref is 3.3V as you can see from the console log I posted last time.Also I use SWD interface.
I'm very confused about that why I can download code using J-Flash but failed when use J-commander.
Hello
You said you changed the "JLinkDevices.xml of jlink", how about do not change it, also use the latest J-commander .
About this question “I'm very confused about that why I can download code using J-Flash but failed when use J-commander.”, how about also ask Segger customer support, maybe they know it well.
https://www.segger.com/support/technical-support/
BR
Alice
Hello,
How about update the debug firmware, and check whether Debug probe recognized by Device Manger of PC.
Does your board is Demo board from NXP or custom board?
BR
Alice
fist,thanks for your reply.
I already have given up trying to use the DAP probe,and use a jlink probe instead.But there still one problem:I can't load my program into a QSPI flash using GUI FLASH TOOL while it's OK with Jlink command.
Hello,
Please show your detail steps with screenshot or vedio.
Also,I have aready modified the JLinkDevices.xml of jlink like:
I can load my program using J-Flash tool.
But it's true that it may be failed when using J-command.Is this the reason to fail to load program using GUI Flash tool of MCUXpresso IDE?
Hello,
""But it's true that it may be failed when using J-command.Is this the reason to fail to load program using GUI Flash tool of MCUXpresso IDE?
->> Maybe, while there isn't this board , I cant' test on my hand, because we are working at home due to COVID-19.
Please show the debug log on Console view.
And try change to another new workspace of ide, and open a simple SDK demo, build, check whether can debug well, then test program using GUI. Also pay attention erase flash before program:
BR
Alice
Hi,
you said "pay attention to erase the flash before program",do you means to check the "Enable erase all flash banks" box,like:
The debug log on console view is listed below:
Executing flash operation 'Program' (Program executable into flash weld_power.axf) - Tue May 31 08:16:54 CST 2022
Checking MCU info...
Scanning for targets...
Executing flash action...
SEGGER J-Link Commander V7.54 (Compiled Sep 1 2021 10:47:47)
DLL version V7.54, compiled Sep 1 2021 10:46:27
J-Link Command File read successfully.
Processing script file...
J-Link Commander will now exit on Error
J-Link connection not established yet but required for command.
Connecting to J-Link via USB...O.K.
Firmware: J-Link V11 compiled Apr 27 2022 16:36:21
Hardware version: V11.00
S/N: xxxxxxx
License(s): GDB, JFlash, FlashDL, RDI, FlashBP
VTref=3.328V
Target connection not established yet but required for command.
Device "MIMXRT1052XXXXA" selected.
Connecting to target via SWD
Found SW-DP with ID 0x0BD11477
DPIDR: 0x0BD11477
Scanning AP map to find all available APs
AP[1]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x04770041)
Iterating through AP map to find AHB-AP to use
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FD000
CPUID register: 0x411FC271. Implementer code: 0x41 (ARM)
Found Cortex-M7 r1p1, Little endian.
FPUnit: 8 code (BP) slots and 0 literal slots
CoreSight components:
ROMTbl[0] @ E00FD000
ROMTbl[0][0]: E00FE000, CID: B105100D, PID: 000BB4C8 ROM Table
ROMTbl[1] @ E00FE000
ROMTbl[1][0]: E00FF000, CID: B105100D, PID: 000BB4C7 ROM Table
ROMTbl[2] @ E00FF000
ROMTbl[2][0]: E000E000, CID: B105E00D, PID: 000BB00C SCS-M7
ROMTbl[2][1]: E0001000, CID: B105E00D, PID: 000BB002 DWT
ROMTbl[2][2]: E0002000, CID: B105E00D, PID: 000BB00E FPB-M7
ROMTbl[2][3]: E0000000, CID: B105E00D, PID: 000BB001 ITM
ROMTbl[1][1]: E0041000, CID: B105900D, PID: 001BB975 ETM-M7
ROMTbl[1][2]: E0042000, CID: B105900D, PID: 004BB906 CTI
ROMTbl[0][1]: E0040000, CID: B105900D, PID: 000BB9A9 TPIU-M7
ROMTbl[0][2]: E0043000, CID: B105F00D, PID: 001BB101 TSG
Cache: Separate I- and D-cache.
I-Cache L1: 32 KB, 512 Sets, 32 Bytes/Line, 2-Way
D-Cache L1: 32 KB, 256 Sets, 32 Bytes/Line, 4-Way
Cortex-M7 identified.
Reset delay: 0 ms
Reset type NORMAL: Resets core & peripherals via SYSRESETREQ & VECTRESET bit.
ResetTarget() start
ResetTarget() end
AfterResetTarget() start
AfterResetTarget() end
PC = 60002360, CycleCnt = 00000000
R0 = 60002361, R1 = 20203A58, R2 = 60002361, R3 = 202051F0
R4 = 60002000, R5 = A63FEB26, R6 = 00200300, R7 = 000000F0
R8 = 401F4470, R9 = 20203A00, R10= A63FEB26, R11= 00000000
R12= 000001FE
SP(R13)= 20020000, MSP= 20020000, PSP= 20020000, R14(LR) = 00211A41
XPSR = 41000000: APSR = nZcvq, EPSR = 01000000, IPSR = 000 (NoException)
CFBP = 00000000, CONTROL = 00, FAULTMASK = 00, BASEPRI = 00, PRIMASK = 00
FPS0 = 00000000, FPS1 = 00000000, FPS2 = 00000000, FPS3 = 00000000
FPS4 = 00000000, FPS5 = 00000000, FPS6 = 00000000, FPS7 = 00000000
FPS8 = 00000000, FPS9 = 00000000, FPS10= 00000000, FPS11= 00000000
FPS12= 00000000, FPS13= 00000000, FPS14= 00000000, FPS15= FFFFFFFF
FPS16= 00000000, FPS17= 00000000, FPS18= 00000000, FPS19= 00000000
FPS20= 00000000, FPS21= 00000000, FPS22= 00000000, FPS23= 00000000
FPS24= 00000000, FPS25= 00000000, FPS26= 00000000, FPS27= 00000000
FPS28= 00000000, FPS29= 00000000, FPS30= 00000000, FPS31= FFFFFFFF
FPSCR= 00000000
Downloading file [E:\XTProj\nxp\weld_power\Debug\weld_power.hex]...
****** Error: Timeout while preparing target, core does not stop. (PC = 0x2000017A, XPSR = 0x41000000, SP = 0x20000B18)!
Failed to initialize RAMCodeTimeout while preparing target, core does not stop. (PC = 0x2000017A, XPSR = 0x41000000, SP = 0x20000B18)!
Failed to initialize RAMCode
Unspecified error -1
Script processing completed.
Unable to perform operation!
Command failed with exit code 1
I just click the GUI FLASH TOOL icon,then a dialog apears:
then click the run button on following picture.