I just did a new install of MCUXpresso IDE 10.2.0 with SDK_2.2_MKL16Z128xxx4 on Windows 10.
According to https://www.nxp.com/docs/en/user-guide/MCUXpresso_IDE_User_Guide.pdf , "MCUXpresso IDE is based on the Eclipse IDE and includes the industry standard ARM GNU toolchain."
I tried opening a project for KL16Z128 and compiling. I get an error saying it cannot find the "make" command in PATH.
Clearly I do not have a correct install of all the needed software.
Are there some directions online to take me from a clean Win10 system with no dev software, to a working MCUXpresso system including some sort of working toolchain to compile the code eg. GNU C compiler? I seem to have skipped some steps somewhere, but don't see clear instructions about installing everything from scratch.
Solved! Go to Solution.
The IDE comes with all the necessary tools, including make. I think your KL16Z project is configured for a different setup or IDE? Can you create a new project from of the KL16 SDK you have installed (Quickstart Panel, use 'New project...'):
I hope this helps,
Erich
I am having a similar issue trying to import a KDS project into MCUxpresso IDE, it thows me the following error:
any solution to this?
Hi @GtrejoS ,
if you want (and need) to use Kinetis Design Studio projects in MCUXpresso IDE, you need to install extra plugins.
See https://mcuoneclipse.com/2017/04/02/mcuxpresso-ide-importing-kinetis-design-studio-projects/ for details.
Going forward, keep in mind that KDS is legacy and the recommendation is to use native MCUXpresso projects instead.
I hope this helps,
Erich
KDS and MCUXpresso projects are not compatible, so, while you can import the projects from KDS, the setup is entirely different. You’ll have to create a new project and copy your sources across.
Hi Erich,
I have installed MCUXpresso and imported SKD example about FRDMK66_freedom_bootloader, but when I try to compile I have an error on file "fat_directory_entry.h" that the include file wchar.h do not exists.
Also in C/C++ General -> Paths and Symbols -> GNUC I read below "Using relative paths is ambiguos and not recommended. It can cause unexpected effects" , in MCUXpresso previous version this it was not neccesary to configure.
Where I'm wronging ?
Thanks for helps
Marco
The IDE comes with all the necessary tools, including make. I think your KL16Z project is configured for a different setup or IDE? Can you create a new project from of the KL16 SDK you have installed (Quickstart Panel, use 'New project...'):
I hope this helps,
Erich
Thank you for your reply. Yes, a new project compiles as expected. My problem was in the older project being configured differently.