Hello,
I have the exact same issue as reported in that thread :
https://community.nxp.com/t5/MCUXpresso-IDE/MCUXPresso-Debug-mode-Variables-Watch-abnormal-on-none-3...
My board is 1061xxxxA and I have Mcuxpresso 11.5.0 Build 7232.
Here's an example of my issue with a struct st_Status with type ST_LIB_STATUS. When initialized with zeroes, memory is correct (only zeros at correspoding address) but field u8_ConsoStatus is different from zero according to variables watcher.
Then I unpack some dummy data in my struct (only 0xFF). Then again, data in memory watcher are correct (0303FFFF, my unpack is not trivial and that is in deed the expected result) but variables watchers show different data.
From what I understand from debug logs, GDB also sees correct data :
184,956 816^done,value="{u8_Heartbeat = 255 '\303\277', u8_FsmStatus = 255 '\303\277', u8_A\
cStatus = 3 '\\003', u8_ConsoStatus = 3 '\\003'}"
I already tried to disable "Live Variables service" without any luck (solution from this tread :https://community.nxp.com/t5/MCUXpresso-IDE/MCUX-11-0-0-Variables-view-has-blank-contents/m-p/949322 )
Any help would be greatly appreciated !
Kind regards.
Solved! Go to Solution.
The solution was to delete .launch file.