MCUXPRESSO Can't debug with opensda with Jlink firmware

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXPRESSO Can't debug with opensda with Jlink firmware

1,387件の閲覧回数
ConstYu
NXP Employee
NXP Employee

i am debugging KW36 demo code with MCUXPRESSO , when i create a new project, it always report below error, my customer also feedback they have this problems. i also noticed there are many user feedback same issue, i tried the methods in those post, but no one does work. 

attached file is source code of my project, the kw36 sdk version is 2.2.0. need great support.

Capture.PNG

ラベル(1)
0 件の賞賛
返信
1 返信

1,231件の閲覧回数
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

Also, did you flashed some example with low power functionality before? Are you sure that your device it's not going to low power?

I also experienced something similar, but it would seem to be with certain build options as I built the SDK with all the IDE's.

Nonetheless, if you will use it with MCUXpresso, have you tried downloading the SDK just for the MCUXpresso IDE? I was able to run and debug the examples building the SDK for that single IDE. I'll keep looking for the other behavior, still could you please try this ?

Hope it helps

Regards,

Estephania

0 件の賞賛
返信