MCUXPRESSO 11.7.1 Jenkins Build Does Not work imxrt1062

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCUXPRESSO 11.7.1 Jenkins Build Does Not work imxrt1062

251 次查看
anthonygarza
Contributor I

I have been beating my head against this wall for far to long. Why even have a command line application if it does not work. It seems that it is trying to pop a window when it is ran from the command line. I can not figure out why.
Things I have tried.

1. reinstalling mcuxpresso MULTIPLE TIMES WITH MULTIPLE VERSIONS!!!!!!

2 reinstalling and configuring JENKINS

3. logging into the JENKINS USER and running mcuxpresso to ensure that the sdk was installed.

4. building from the command line as the context of the jenkins usr.( works) So why doesnt mcuxpresso work??? Why does it constantly give these same cryptic errors??????

The frustration is real here. 

input:

 

#!/bin/sh
ls -a
cd ~
ls -a
echo "Printing where I am"
pwd
echo "printing HOME"
printenv HOME
cd workspace
ls -a
echo "who I am"
whoami
echo "sdk env"
printenv MCUXPRESSOIDE_SDK_INSTALL
sudo /usr/local/mcuxpressoide/ide/mcuxpressoide -noSplash -application org.eclipse.cdt.managedbuilder.core.headlessbuild --launcher.suppressErrors -data "../testBuild/." -remove HWCBBuild/HWController_1062
echo "REMOVE PROJECT COMPLETE "
sudo /usr/local/mcuxpressoide/ide/mcuxpressoide -noSplash -application org.eclipse.cdt.managedbuilder.core.headlessbuild --launcher.suppressErrors -data "../testBuild/." -import HWCBBuild/HWController_1062
echo "Add PROJECT COMPLETE "
sudo /usr/local/mcuxpressoide/ide/mcuxpressoide --launcher.suppressErrors -nosplash -debug -consoleLog -application org.eclipse.cdt.managedbuilder.core.headlessbuild -no-indexer -data "../testBuild/." -build HWController_1062/DEBUG_MARK_1_9_HW_BETA_BOARD_REV_B

 

output:

 

!ENTRY com.nxp.mcuxpresso.core.datamodels 1 0 2024-04-18 14:54:34.954
!MESSAGE The device 'MIMXRT1062xxxxA' (version='1.0.0') from SDK 'SDK_2.x_MIMXRT1062xxxxA' (version='2.12.1', build='632 2022-09-26') will be installed.
log4j:WARN No appenders could be found for logger (org.eclipse.xtext.ui.internal.Activator).
log4j:WARN Please initialize the log4j system properly.
log4j:WARN See http://logging.apache.org/log4j/1.2/faq.html#noconfig for more info.
Unable to init server: Could not connect: Connection refused

!ENTRY org.eclipse.osgi 4 0 2024-04-18 14:54:43.618
!MESSAGE Application error
!STACK 1
org.eclipse.swt.SWTError: No more handles [gtk_init_check() failed]
	at org.eclipse.swt.SWT.error(SWT.java:4944)
	at org.eclipse.swt.widgets.Display.createDisplay(Display.java:1154)
	at org.eclipse.swt.widgets.Display.create(Display.java:1078)
	at org.eclipse.swt.graphics.Device.<init>(Device.java:168)
	at org.eclipse.swt.widgets.Display.<init>(Display.java:630)
	at org.eclipse.swt.widgets.Display.<init>(Display.java:621)
	at org.eclipse.swt.widgets.Display.getDefault(Display.java:2347)
	at org.eclipse.jface.preference.PreferenceConverter.<clinit>(PreferenceConverter.java:100)
	at org.eclipse.ui.texteditor.AbstractDecoratedTextEditorPreferenceConstants.initializeDefaultValues(AbstractDecoratedTextEditorPreferenceConstants.java:745)
	at org.eclipse.ui.editors.text.TextEditorPreferenceConstants.initializeDefaultValues(TextEditorPreferenceConstants.java:291)
	at org.eclipse.ui.internal.editors.text.EditorsPluginPreferenceInitializer.initializeDefaultPreferences(EditorsPluginPreferenceInitializer.java:44)
	at org.eclipse.core.internal.preferences.PreferenceServiceRegistryHelper$1.run(PreferenceServiceRegistryHelper.java:307)
	at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
	at org.eclipse.core.internal.preferences.PreferenceServiceRegistryHelper.runInitializer(PreferenceServiceRegistryHelper.java:310)
	at org.eclipse.core.internal.preferences.PreferenceServiceRegistryHelper.applyRuntimeDefaults(PreferenceServiceRegistryHelper.java:134)
	at org.eclipse.core.internal.preferences.PreferencesService.applyRuntimeDefaults(PreferencesService.java:374)
	at org.eclipse.core.internal.preferences.DefaultPreferences.applyRuntimeDefaults(DefaultPreferences.java:225)
	at org.eclipse.core.internal.preferences.DefaultPreferences.load(DefaultPreferences.java:279)
	at org.eclipse.core.internal.preferences.EclipsePreferences.create(EclipsePreferences.java:367)
	at org.eclipse.core.internal.preferences.EclipsePreferences.internalNode(EclipsePreferences.java:620)
	at org.eclipse.core.internal.preferences.EclipsePreferences.node(EclipsePreferences.java:759)
	at org.eclipse.core.internal.preferences.AbstractScope.getNode(AbstractScope.java:41)
	at org.eclipse.core.runtime.preferences.DefaultScope.getNode(DefaultScope.java:77)
	at org.eclipse.ui.preferences.ScopedPreferenceStore.getDefaultPreferences(ScopedPreferenceStore.java:222)
	at org.eclipse.ui.preferences.ScopedPreferenceStore.getPreferenceNodes(ScopedPreferenceStore.java:251)
	at org.eclipse.ui.preferences.ScopedPreferenceStore.contains(ScopedPreferenceStore.java:308)
	at org.eclipse.ui.texteditor.ChainedPreferenceStore.getVisibleStore(ChainedPreferenceStore.java:465)
	at org.eclipse.ui.texteditor.ChainedPreferenceStore.contains(ChainedPreferenceStore.java:141)
	at org.eclipse.xtext.builder.EclipseOutputConfigurationProvider.getBoolean(EclipseOutputConfigurationProvider.java:173)
	at org.eclipse.xtext.builder.EclipseOutputConfigurationProvider.createAndOverlayOutputConfiguration(EclipseOutputConfigurationProvider.java:144)
	at org.eclipse.xtext.builder.EclipseOutputConfigurationProvider.createAndOverlayOutputConfiguration(EclipseOutputConfigurationProvider.java:153)
	at org.eclipse.xtext.builder.EclipseOutputConfigurationProvider.getOutputConfigurations(EclipseOutputConfigurationProvider.java:112)
	at org.eclipse.xtext.builder.BuilderParticipant.getOutputConfigurations(BuilderParticipant.java:652)
	at org.eclipse.xtext.builder.BuilderParticipant.build(BuilderParticipant.java:247)
	at org.eclipse.xtext.builder.impl.RegistryBuilderParticipant$DeferredBuilderParticipant.build(RegistryBuilderParticipant.java:164)
	at org.eclipse.xtext.builder.impl.RegistryBuilderParticipant.build(RegistryBuilderParticipant.java:70)
	at org.eclipse.xtext.builder.impl.XtextBuilder.doBuild(XtextBuilder.java:525)
	at org.eclipse.xtext.builder.impl.XtextBuilder.addInfosFromTaskAndBuild(XtextBuilder.java:455)
	at org.eclipse.xtext.builder.impl.XtextBuilder.fullBuild(XtextBuilder.java:562)
	at org.eclipse.xtext.builder.impl.XtextBuilder.build(XtextBuilder.java:333)
	at org.eclipse.core.internal.events.BuildManager$2.run(BuildManager.java:1024)
	at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:45)
	at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:254)
	at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:427)
	at org.eclipse.core.internal.events.BuildManager.build(BuildManager.java:626)
	at org.eclipse.core.internal.resources.Project$1.run(Project.java:568)
	at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2380)
	at org.eclipse.core.internal.resources.Project.internalBuild(Project.java:606)
	at org.eclipse.core.internal.resources.Project.build(Project.java:126)
	at org.eclipse.cdt.managedbuilder.core.ManagedBuildManager$2.buildProject(ManagedBuildManager.java:4534)
	at org.eclipse.cdt.managedbuilder.core.ManagedBuildManager$2.run(ManagedBuildManager.java:4511)
	at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2380)
	at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2400)
	at org.eclipse.cdt.managedbuilder.core.ManagedBuildManager.buildConfigurations(ManagedBuildManager.java:4543)
	at org.eclipse.cdt.managedbuilder.core.ManagedBuildManager.buildConfigurations(ManagedBuildManager.java:4423)
	at org.eclipse.cdt.managedbuilder.internal.core.HeadlessBuilder.buildConfigurations(HeadlessBuilder.java:322)
	at org.eclipse.cdt.managedbuilder.internal.core.HeadlessBuilder.start(HeadlessBuilder.java:710)
	at org.eclipse.cdt.managedbuilder.internal.headlessbuilderapp.HeadlessBuilderWrapper.start(HeadlessBuilderWrapper.java:131)
	at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:203)
	at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:136)
	at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104)
	at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:402)
	at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:255)
	at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
	at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke(Unknown Source)
	at java.base/jdk.internal.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source)
	at java.base/java.lang.reflect.Method.invoke(Unknown Source)
	at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:659)
	at org.eclipse.equinox.launcher.Main.basicRun(Main.java:596)
	at org.eclipse.equinox.launcher.Main.run(Main.java:1467)
	at org.eclipse.equinox.launcher.Main.main(Main.java:1440)
Mcuxpressoide:
An error has occurred. See the log file
/var/lib/jenkins/testBuild/.metadata/.log.
Start VM: /usr/local/mcuxpressoide-11.7.1_9221/ide//jre/bin/java
-Dosgi.requiredJavaVersion=11
-Xms256m
-Xmx3072m
-Djava.net.useSystemProxies=true
-Dnashorn.args=--no-deprecation-warning --language=es6
-jar /usr/local/mcuxpressoide-11.7.1_9221/ide//plugins/org.eclipse.equinox.launcher_1.6.400.v20210924-0641.jar
-os linux
-ws gtk
-arch x86_64
-launcher /usr/local/mcuxpressoide-11.7.1_9221/ide/mcuxpressoide
-name Mcuxpressoide
--launcher.library /usr/local/mcuxpressoide-11.7.1_9221/ide//plugins/org.eclipse.equinox.launcher.gtk.linux.x86_64_1.2.500.v20220509-0833/eclipse_11701.so
-startup /usr/local/mcuxpressoide-11.7.1_9221/ide//plugins/org.eclipse.equinox.launcher_1.6.400.v20210924-0641.jar
--launcher.overrideVmargs
-exitdata 2001d
-debug
-consoleLog
-application org.eclipse.cdt.managedbuilder.core.headlessbuild
-no-indexer
-data ../testBuild/.
-build HWController_1062/DEBUG_MARK_1_9_HW_BETA_BOARD_REV_B
-vm /usr/local/mcuxpressoide-11.7.1_9221/ide//jre/bin/java
-vmargs
-Dosgi.requiredJavaVersion=11
-Xms256m
-Xmx3072m
-Djava.net.useSystemProxies=true
-Dnashorn.args=--no-deprecation-warning --language=es6
-jar /usr/local/mcuxpressoide-11.7.1_9221/ide//plugins/org.eclipse.equinox.launcher_1.6.400.v20210924-0641.jar 
Build step 'Execute shell' marked build as failure
Finished: FAILURE

 

 

0 项奖励
回复
1 回复

72 次查看
brillians
Contributor I

I ran into this same issue using Jenkins with MCUXpresso (headless). I was able to fix it by following the first reply from this post:


https://community.nxp.com/t5/MCUXpresso-IDE/Ubuntu-cmd-build-No-more-handles-gtk-init-check-failed/m...

The solution was to delete all of the xtext references from my .project file.

0 项奖励
回复