MCUExpression cannot find the CMSIS-DAP probes

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUExpression cannot find the CMSIS-DAP probes

1,253 Views
Desmond_lim
Contributor III

This has been bothered me for a week after reading the forum for solution on this issue that also happened to me as well all of the sudden.

Desmond_lim_0-1669017253864.png

This happen with MCUXpressor IDE build v11.5.0. The problem happened after I reboot my PC and there was no upgrade or anything on my PC or my board. I checked the forum and the similar thing is happening to the other guy but my case is different because I did not connect to the JLink but via the mini USB on the board. Neither do I delete any JLink files. It just happened after I reboot my PC. I am not sure if the CMSIS-DAP device driver is corrupted or not because I was working on  the USB DFU SDK program before that. 

I need this to be resolved asap because I basically cannot work on anything under this condition. Please help.

 

Tags (2)
0 Kudos
Reply
3 Replies

1,227 Views
Desmond_lim
Contributor III

I changed the device drivers for DAP-CMSIS, USB Serial and WebUsb to the microsoft instead of NXP in the device driver. Then, everything becomes ok. I was a bit worried because of one solution was suggesting to reinstall the entire OS (Windows 10). So far this has worked for me but I am not sure if this is a proper solution or any hidden issues on that.

0 Kudos
Reply

1,246 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Unfortunately, it's very difficult to debug these kind of issues over a forum. I'd say something happened with your hardware. Also, it might help if you'd take a look at the guide written for MIMXRT1170-EVK - https://community.nxp.com/t5/Blogs/Overview-of-using-the-MIMXRT1170-EVK-with-MCUXpresso-IDE/ba-p/124...

Regards,
MCUXpresso IDE Support

0 Kudos
Reply

1,250 Views
Desmond_lim
Contributor III

I have reinstalled the CMSIS-DAP driver. It has the same problem as well. I am fully out of my wits.

The CMSIS-DAP driver from NXP site

Desmond_lim_0-1669021797776.png

 

The problem still persist.

Desmond_lim_1-1669021839025.png

 

0 Kudos
Reply