MCU Xpresso blocks the MCU from free running

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCU Xpresso blocks the MCU from free running

ソリューションへジャンプ
942件の閲覧回数
Catosh
Contributor IV

Long story short: 
when I debug, the MCU is able to run.
Then I terminate the debug session, remove the debugger probe, perform a power cycle and the MCU is not able to run. 
Is there some command to remove the debugging probe and terminate the debug session leaving the MCU in free running mode from MCU Xpresso?

B.R.

L.T.

1 解決策
792件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Which version of the IDE are you using?

Are you using semihosting calls (printf(), etc)? If so, then they can block the microcontroller if no debug probe is attached.

Erich

元の投稿で解決策を見る

3 返答(返信)
792件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

The easiest way to "disable" semihosting printf's is to reconfigure your project to link against a "nohost" variant of the C library. For SDK based projects, you can also reconfigure output in many cases so it is sent over a UART rather than the debug probe.

But alternatively, MCUXpresso IDE v10.1 allows projects which contain a hard fault handler that can trap and "recover" from a semihosted operation taking place when the debugger is not connected.

For more information please see chapter 13, "C/C++ Library Support" of the MCUXpresso IDE v10.1 User Guide.

Regards,

MCUXpresso IDE Support

0 件の賞賛
793件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Which version of the IDE are you using?

Are you using semihosting calls (printf(), etc)? If so, then they can block the microcontroller if no debug probe is attached.

Erich

792件の閲覧回数
Catosh
Contributor IV

Hello Erich, 

Actually, yes. I 'll remove then and come back to the post!

#edit:

BTW is there some smart way to remove the semihosting calls, like undef from the preprocessor windows in settings menu?

0 件の賞賛