LPC54608 board doesnt see any debug probes

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54608 board doesnt see any debug probes

Jump to solution
2,311 Views
k2
Contributor III

Bought a LPC54608 board,

installed IDE, etc.

compiled an example SDK I2C example project

When i goe to download it i get

"No compatible probes available. They may be disabled, disconnected, not powered, already in use or not compatible with this target."

How do i get the default Link2 probe to show up in discovery ?

I see the LPC-LINK2 CMSIS-DAP V5.173 enumerated under devices in Win7.

The canned DEMO works fine - so i know the board is good.

0 Kudos
1 Solution
1,748 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Kevin,

      Thanks a lot for your updated information and that's very good to hear you make it working.

      If your problem is solved, please help to mark the correct answer, just to close this question, thank you!

    


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
5 Replies
1,748 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Kevin King,

   Thank you for your interest in NXP LPC and MCUXpresso IDE, I would like to provide service for you.

    Now, please follow my steps and try again.

1. I find your CMSIS DAP version is a little old

   You can update it at first.

  1) download lpcscrypt tool and install it.

     LPCScrypt v1.8.2|NXP 

  2) power down the LPC54608 board

    Short JP5

    Use the USB cable connect J8.

    Open PC: Control Panel\Hardware and Sound\Devices and Printers

   You will find your board is named as LPC, just like this picture:

pastedImage_2.png

  3)  Open LPCScript, program LPC-LINK2 with CMSIS-DAP window

  

14.jpg

pastedImage_5.png

Press any key, wait the write finished.

pastedImage_6.png

 4) Power off the boad, remove the short between JP5, check PC: Control Panel\Hardware and Sound\Devices and Printers

15.jpg

Until now, your CMSIS DAP is updated as the new version.

2. Open the SDK I2C example project with MCUXpress

pastedImage_8.png

1.) RUN->debug configuration

    Please delete the two files under MCU Application

pastedImage_9.png

2). Build the project

3). Click debug

pastedImage_10.png

  You will get this window:

pastedImage_14.png

Press OK button

You will enter the debug mode:

pastedImage_15.png

Please follow my above steps, and try again.

Any question, just let me know!

@ZhangJennie
Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,748 Views
k2
Contributor III

Kerry,

I got it to connect one time after deleting and re-installing the IDE and etc.

I see the REDLINK server not active (red chain symbol) ...

doesn't that have to be active to connect ?

It seems after I first launch MCUxpresso it is RED and active - after I select a project - it goes inactive ?

and doesn't connect.

Got any clues ?

I turned off my wirewall just in case ... didn't help.

Kevin

0 Kudos
1,748 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Kevin King,

     Don't use the REDLINK, just follow my method which is post in the above.

    Which step you are stopping? You can also post some pictures on your side.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,748 Views
k2
Contributor III

Kerry,

Got everything working now.

Re-installed everything ...

That was what fixed it.

Thanks for helping.

Kevin

Sent from my iPhone

0 Kudos
1,749 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Kevin,

      Thanks a lot for your updated information and that's very good to hear you make it working.

      If your problem is solved, please help to mark the correct answer, just to close this question, thank you!

    


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos