Bought a LPC54608 board,
installed IDE, etc.
compiled an example SDK I2C example project
When i goe to download it i get
"No compatible probes available. They may be disabled, disconnected, not powered, already in use or not compatible with this target."
How do i get the default Link2 probe to show up in discovery ?
I see the LPC-LINK2 CMSIS-DAP V5.173 enumerated under devices in Win7.
The canned DEMO works fine - so i know the board is good.
已解决! 转到解答。
Hello Kevin,
Thanks a lot for your updated information and that's very good to hear you make it working.
If your problem is solved, please help to mark the correct answer, just to close this question, thank you!
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Kevin King,
Thank you for your interest in NXP LPC and MCUXpresso IDE, I would like to provide service for you.
Now, please follow my steps and try again.
1. I find your CMSIS DAP version is a little old
You can update it at first.
1) download lpcscrypt tool and install it.
2) power down the LPC54608 board
Short JP5
Use the USB cable connect J8.
Open PC: Control Panel\Hardware and Sound\Devices and Printers
You will find your board is named as LPC, just like this picture:
3) Open LPCScript, program LPC-LINK2 with CMSIS-DAP window
Press any key, wait the write finished.
4) Power off the boad, remove the short between JP5, check PC: Control Panel\Hardware and Sound\Devices and Printers
Until now, your CMSIS DAP is updated as the new version.
2. Open the SDK I2C example project with MCUXpress
1.) RUN->debug configuration
Please delete the two files under MCU Application
2). Build the project
3). Click debug
You will get this window:
Press OK button
You will enter the debug mode:
Please follow my above steps, and try again.
Any question, just let me know!
@ZhangJennie
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Kerry,
I got it to connect one time after deleting and re-installing the IDE and etc.
I see the REDLINK server not active (red chain symbol) ...
doesn't that have to be active to connect ?
It seems after I first launch MCUxpresso it is RED and active - after I select a project - it goes inactive ?
and doesn't connect.
Got any clues ?
I turned off my wirewall just in case ... didn't help.
Kevin
Hello Kevin King,
Don't use the REDLINK, just follow my method which is post in the above.
Which step you are stopping? You can also post some pictures on your side.
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Kevin,
Thanks a lot for your updated information and that's very good to hear you make it working.
If your problem is solved, please help to mark the correct answer, just to close this question, thank you!
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------