Dear Sirs,
I'm trying to use a LPC4088 Quickstart board by Embedded Artists using the IDE MCUXpresso 10.1.1.
I've used the same board on LPCXpresso and worked well.
When I try to debug the code by using the USB debugger on board this message is shown by MCUXpresso.
I don't understand the reason why it doesn't work properly.
The project is attached to this e-mail
Best regards
解決済! 解決策の投稿を見る。
I see no problems debugging a simple project created with the IDE's new project wizard on the Embedded Artist LPC4088 quickstart board that I have here via the onboard debug USB connector.
I would suggest starting off by booting the board into ISP mode before trying to make a debug connection. To do this press and hold the "User" button, press and release the "Reset" button, then release the "User" button. Background information on this can be found in the FAQ at: Regaining debug access to target MCU
It might also be worth checking if your board has the latest probe firmware installed. For more details see the information that Embedded Artists publish at:
Regards,
MCUXpresso IDE Support
Thanks a lot for your kind support.
I see no problems debugging a simple project created with the IDE's new project wizard on the Embedded Artist LPC4088 quickstart board that I have here via the onboard debug USB connector.
I would suggest starting off by booting the board into ISP mode before trying to make a debug connection. To do this press and hold the "User" button, press and release the "Reset" button, then release the "User" button. Background information on this can be found in the FAQ at: Regaining debug access to target MCU
It might also be worth checking if your board has the latest probe firmware installed. For more details see the information that Embedded Artists publish at:
Regards,
MCUXpresso IDE Support